STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! question about STM32MP157C-DK2

Hi,My test kit is STM32MP157C-DK2 and kenerl version is 5.10.10.I tried to monitor falling edge event on PD.1, with command "gpiomon --falling-edge gpiochip3 1". It is faile and and the log in the attachment.Then I disable "hdmi-transmitter@39" in "s...

zqizh.1 by Associate III
  • 2135 Views
  • 2 replies
  • 0 kudos

Error Flashing first partition: Hello, I have a custom board with STM32mp157c and i'm trying to load the u-boot for ddr testing. I created u-boot basic defconfig with ddr_interactive=1 and

a tsv file with #Opt id Name Type IP Offset Binary - 0x01 fsbl Binary none 0x00000000 u-boot-spl.stm32 I got different error messages:stm32CubeProgrammer on windows:sending a dfu end of download request DFU status = 0 DFU State = 7 DFU status =...

Lmoio.1 by Senior
  • 1823 Views
  • 3 replies
  • 0 kudos

STM32MP1 using FMC from CM4 core

We are using the STM32MP15 ecosystem 2.1.0 and buildroot build flow for a custom board.  The custom board uses the FMC peripheral to connect to three FPGAs using an SRAM/PSRAM interface.  We have successfully implemented this interface on the CA7 sid...

MCarl.3 by Associate II
  • 2659 Views
  • 3 replies
  • 2 kudos

Why MPU's ST support is so slowly...

Could you please explain me why ST support is so slowly... I'm starting with STM32MP1xx MPUs hoping, that ST support will be fast and specific. But currently answer for even simple (and stupid) questions need to be wait for unpredictable time...We ne...

ASkri.1 by Senior
  • 1816 Views
  • 3 replies
  • 0 kudos

Configure Serdev on USART 3

Helllo i configurated my Device tree so i a can use my USART3 as a serdev. But when i run "cat /proc/tty/driver/stm32-usart". i can see my serial port but my RTS pin is missing. I configurated my device tree like this:&usart3 { pinctrl-names = "defau...

SAman.1 by Associate III
  • 2093 Views
  • 1 replies
  • 0 kudos