STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ethernet PHY does not work with 100 Mbps Full Duplex but works with 10 Mbps Full Duplex

Hello,we want to bring up our own board with STM32MP and ethernet phy LAN8720 (10/100 Mbps).Seems that kernel is recognizing ethernet phy on boot up and configure it with 100 Mbps Full Duplex.[ 2.907461] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi ...

DmnSd by Associate III
  • 4740 Views
  • 2 replies
  • 0 kudos

Resolved! Where this remoteproc node is defined and with what syntax? Can I add multiples?

I am trying to have firmware_m4_X running on M4 core, and fimware_A7_Linux, runnin on Linux and them intercommunicating via RPMSx. If I upload them separately they work fine but after board reboot I want these two images to be started automatically. ...

Resolved! Is there a chance to perhaps get a video tutorials, of step-by-step for kernel-configuration-uploading ?

I have two codes running (on stm32mp157f-Dk2) successfully one is running on M4+freeRTOS another on A7+Linux, they are intercommunicating via RPMSGx. The problem is that after power-loss or reboot, I want both of my programs starting automatically an...

Resolved! C++ Compiler support on STM32MPU

Hi,I would like to compile a user space c++ application on the STM32MP157C-DK2. Is it possible to install GCC or G++ on the board?I tried installing them via apt-get but seems like there is not any package with name gcc or g++.How can i install it an...

NPal.2 by Senior
  • 2418 Views
  • 2 replies
  • 0 kudos