STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Close the device, fuse under op-tee?

I'm having trouble closing a device as per the recommended method.STM32MP> fuse read 0 0                                                         Reading bank 0:                                                                Word 0x00000000: 00000017 ...

Resolved! Missing /dev/ttyRPMSG0

Hi,After installing and running the latest, OpenStLinux discovered a problem with M4. Firmware is loading fine, but the system doesn't create /dev/ttyRPMSGx channel. What is changed in comparison to the dunfell?[ 2399.320707] remoteproc remoteproc0: ...

MWoło.2 by Senior III
  • 4227 Views
  • 7 replies
  • 0 kudos

Resolved! STM32MP1 OTP word 10 and 11

Hi, I'm trying to leverage the capability of lower words to be programmed once to one bit by bit to implement a sort of "forever growing counter", not sure if there is a proper naming for this.In the lower OTP zone, if I understood correctly, word 10...

Resolved! STM32MP1 DSI voltage level

I would like to clear up some confusion regarding the DSI VIO, the stm32mp157a datasheet mentions "1.2 V I/O for DSI interface" but in the EV1 kit the LCD used (the RK055AHD042-CT, for which it's impossible to find a datasheet for, could that be shar...

arturo182 by Associate II
  • 8273 Views
  • 6 replies
  • 0 kudos

On a linux stm32mp157 system can gpio with pullup or pull-down resistors be configured in user space ? If yes how?

I just spent a day trying to configure a gpio with internal pullup using gpiolib. Could not get it configured. Then spent 2 days with device drivers and device trees, and got it working. Seems insane to me that configuring gpios should be this comple...

Rc.1 by Associate II
  • 6725 Views
  • 6 replies
  • 0 kudos