STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! “Error: failed to download Segment[0]�? Populate the target and boot the image example

“Error: failed to download Segment[0]�?I looked at the other items with the same title but did not see an answer that would help me.I am using the STM32MP157F-DK2The demo code was working when box was openedI tried to run the demo“Populate the target...

JAmia.1 by Associate II
  • 11103 Views
  • 16 replies
  • 0 kudos

Resolved! Start M4 firmware from A7 application

Hi!I am using STM32MP157C-DK2 board to create an application on the screen (using GTK library). My idea is to start coprocessor firmware from the A7 application with the following commands (system commands):int main (int argc, char **argv) { GtkApp...

0693W00000Y92TKQAZ.png
TArre.1 by Associate III
  • 4435 Views
  • 6 replies
  • 1 kudos