cancel
Showing results for 
Search instead for 
Did you mean: 

About handling pins named "Unused"

tatsuya
Associate II

Hi team,

I'm developing a our PCB equipped with STM32MP151AAA3.

Are the following pins named "Unused" okay to remain open?

VDD_Unused

VDD1V2_Unused

VDDA1V8_Unused

Best regard,

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @tatsuya​ 

I recommend reading AN5031.

If you don't want to provision your board for future IC replacement with new features (e.g. use STM32MP157C with DSI interface), the _Unused pin could be left open.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

1 REPLY 1
PatrickF
ST Employee

Hi @tatsuya​ 

I recommend reading AN5031.

If you don't want to provision your board for future IC replacement with new features (e.g. use STM32MP157C with DSI interface), the _Unused pin could be left open.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here