STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use sysvinit in Yocto

I want to use sysinitv instead of systemd . When I add DISTRO_FEATURES_remove = "systemd" in Distro conf ,bitbake stopped whit ERROR: /home/st/openstlinux-5.10-dunfell-mp1-21-11-17/layers/meta-openembedded/meta-initramfs/recipes-core/packagegroups/pa...

Yby.1 by Associate
  • 6809 Views
  • 2 replies
  • 2 kudos

STM32MP1 trying to add GCC

Hello,I have several python modules I am trying to install that require building something in C. I've read through this and completed a build. I got to the part about adding layers and I'm lost. I've not built a distribution using these tools bef...

How can STM32 solutions make your applications smarter, more secure, and more connected?

The STM32 MCU and MPU portfolio brings developers a wide range of design possibilities to make industrial applications smarter, more secure, and more connected.In 2023, we will continue to deliver on that promise.Join us for the STM32 Innovation Live...

0693W00000YAAaZQAX.jpg

ADC in continuous mode only reading once

I am trying to read data using ADC1 continuously and copy it into a buffer via DMA.However, the data is only read and copied once (seemingly correctly), and afterwards nothing happens anymore (data in buffer does not change, ADC1_IRQHandler() is not ...

RPape.1 by Associate II
  • 1707 Views
  • 0 replies
  • 0 kudos

stm32mp1 i2s1 mclk bitrate issue

Hi in one of link https://wiki.st.com/stm32mpu/wiki/I2S_Linux_driver#Short_Descriptioncan i2s1 used for mclk generation, and will the parent clock able to generate mclk for different audio different bitrate,because in dk2 we use i2s2 for mclk generat...

0693W00000aHZLYQA4.png
RRaj.3 by Associate
  • 1016 Views
  • 0 replies
  • 0 kudos