2022-08-10 1:56 AM
Hello everyone ~
My custom board has RGB(LTDC) and HDMI display interfaces.
We want to display same screen on same time.(duplicate mode)
So, LTDC interface connected to local LCD and HDMI transmitter(sii9022).
<dc node of my dts is below ..
<dc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_mx>;
pinctrl-1 = <<dc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ltdc */
port {
#address-cells = <1>;
#size-cells = <0>;
ltdc_ep0_out: endpoint@0 {
reg = <0>;
remote-endpoint = <&sii9022_in>;
};
};
/* USER CODE END ltdc */
};and we can display both screen successfully as below picture.
However, unfortunately my LCD`s resolution is 1280x800.
and linux platform doesn't have this HDMI resolution mode.
so my LCD was displayed as below...
Therefore, I want to add 1280x800 mode to HDMI.
Is there any guide article on wiki?
Thanks a lot !!!
Solved! Go to Solution.
2022-08-26 1:19 AM
2022-08-26 1:13 AM
My clock configuration was problem.
Below linked question was very helpful to me, thanks.
2022-08-26 1:19 AM