STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32MP13 Board bring up issue

We are working on a custom board (based on STM32MP135F-DK) which uses STM32MP131AAE and STPMIC1DPQR PMIC.We are using STM32CubeProgrammer TSV Flashing service to flash the image into eMMC, in this process we are getting a PMIC Panic NOTICE: CPU: STM...

panic error during optee binary update

Getting panic error during optee binary update. We are stuck on this. Kindly provide any guidance. We are using emmc for boot and Two file updating till now. But after fip-stm32mp135f-dk-optee.bin update we are getting this error. Here is the log- NO...

manishee by Associate
  • 1619 Views
  • 1 replies
  • 0 kudos

Break error interrupt in USART

Hello Team, Now I am working on stm32mp133f MCU.  I need to implement break error interrupt in USART. My requirement is when we got 'NULL' data on  RX FIFO . it should generate break interrupt. shall I get this  interrupt with frame error.  

Kaduru by Associate II
  • 3140 Views
  • 4 replies
  • 0 kudos

strex calls DAbt interrupt

Processor stm32mp157it runs Opencv in baremetal modesingle-tasking environment.when calling a methodvoid UMat::addref(){if( u )CV_XADD(&(u->urefcount), 1);}we get DAbt.The disassembler shows a set of instructions 388 CV_XADD(&(u->urefcount), 1);c013c...

Resolved! STM32MP157 GPIO access

Hi team,I have an STM32MP157 board with a Cortex-M4 processor. I have a simple task, which is to toggle the GPIO at maximum speed with accuracy, ensuring that the clock width does not vary.The maximum toggle speed we require is approximately 15ns bet...

kundanJha by Associate II
  • 29442 Views
  • 9 replies
  • 0 kudos