User Activity

I am booting from EMMC with this flash layout./dev/mmcblk1p1 : start= 34, size= 1024, type=8DA63339-0007-60C0-C436-083AC8230908, uuid=077BFE04-5B1A-41F8-8DC2-B47FCC4EA832, name="metadata1"/dev/mmcblk0p2 : start= 1058, size= 1024, type=8DA63339-0007-6...
u-boot yocto build fails with this messagetest -e arch/arm/dts/stm32mp157c-mydemo-mx.dtb || ( \| echo >&2; \| echo >&2 "Device Tree Source (arch/arm/dts/stm32mp157c-mydemo-mx.dtb) is not correctly specified."; \| echo >&2 "Please define 'CONFIG_DEFAU...
flashlayout tsv file not generated using meta-st-stm32mp-addons but images created.What do I need to add to generate the Flashlayout for sdcard?
Doing a build using yocto mickledore it fails with this error message.CMake Error at host/xtest/CMakeLists.txt:3 (include): include could not find requested file: ... /tmp-glibc/work/osd32mp1_brk-ostl-linux-gnueabi/optee-test/3.19.0+gitAUTOINC+ab9863...
I'm building libqmi for the STM32MP157 and getting an error  at this point in the build GISCAN Qmi-1.0.girTraceback (most recent call last):File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-v...