cancel
Showing results for 
Search instead for 
Did you mean: 

STUSB1600 (USB-C) Alternatives

Sindel
Associate

Hey,

I am designing a board based on the STM32MP157F using the OSD32MP157F SOM as a base. I want to have a usb-c connector acting as a host and/or as hs_otg. Reviewing the DK boards schematics I see that the STUSB1600 is being used. I also see on the dts that STUSB1600 is used in conjuction with I2C4. I was wondering whether I can use an alternative like the TPS25820 or other USB-C source controller and if there are any recommendations on this manner, preferably with a compatible or easily portable kernel module.

Any ideas or suggestions are highly appreciated.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.