cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect the printer

macrobert
Associate II

Hi

I got cups and hplip by adding IMAGE_INSTALL_append = "python3-distro cups ghostscript cups-filters hplip"  in local.conf.

but when I run hp-check, there are some errors about missing required dependencies :

 

root@STM32MP1:~# hp-check
/usr/bin/hp-check:685: SyntaxWarning: "is not" with a literal. Did you mean "!="?
  if 'getfacl' not in g and '' is not g and 'file' not in g:
warning: python-dbus not installed.
Saving output in log file: /home/root/hp-check.log

HP Linux Imaging and Printing System (ver. 3.19.12)
Dependency/Version Check Utility ver. 15.1

Copyright (c) 2001-18 HP Development Company, LP
This software comes with ABSOLUTELY NO WARRANTY.
This is free software, and you are welcome to distribute it
under certain conditions. See COPYING file for more details.

Note: hp-check can be run in three modes:
1. Compile-time check mode (-c or --compile): Use this mode before compiling the HPLIP supplied       
tarball (.tar.gz or .run) to determine if the proper dependencies are installed to successfully       
compile HPLIP.                                                                                        
2. Run-time check mode (-r or --run): Use this mode to determine if a distro supplied package (.deb,  
.rpm, etc) or an already built HPLIP supplied tarball has the proper dependencies installed to        
successfully run.                                                                                     
3. Both compile- and run-time check mode (-b or --both) (Default): This mode will check both of the   
above cases (both compile- and run-time dependencies).                                                

Check types:                                                                                          
a. EXTERNALDEP - External Dependencies                                                                
b. GENERALDEP - General Dependencies (required both at compile and run time)                          
c. COMPILEDEP - Compile time Dependencies                                                             
d. [All are run-time checks]                                                                          
PYEXT SCANCONF QUEUES PERMISSION                                                                      

Status Types:
    OK
    MISSING       - Missing Dependency or Permission or Plug-in
    INCOMPAT      - Incompatible dependency-version or Plugin-version

warning: st openstlinux - eglfs - (a yocto project based distro) distro is not found in AUTH_TYPES
warning: 50-3.1-snapshot-20231024 version is not supported. Using 50-6 versions dependencies to verify and install...

---------------
| SYSTEM INFO |
---------------

 Kernel: 5.4.31 #1 SMP PREEMPT Wed May 8 07:13:52 UTC 2024 GNU/Linux
 Host: STM32MP1
 Proc: 5.4.31 #1 SMP PREEMPT Wed May 8 07:13:52 UTC 2024 GNU/Linux
 Distribution: 50 3.1-snapshot-20231024
 Bitness: 32 bit


-----------------------
| HPLIP CONFIGURATION |
-----------------------

HPLIP-Version: HPLIP 3.19.12
HPLIP-Home: /usr/share/hplip
warning: HPLIP-Installation: Auto installation is not supported for 50 distro  3.1-snapshot-20231024 version 

Current contents of '/etc/hp/hplip.conf' file:
# hplip.conf.  Generated from hplip.conf.in by configure.

[hplip]
version=3.19.12

[dirs]
home=/usr/share/hplip
run=/var/run
ppd=/usr/share/ppd/HP
ppdbase=/usr/share/ppd
doc=/usr/share/doc/hplip-3.19.12
html=/usr/share/doc/hplip-3.19.12
icon=/usr/share/applications
cupsbackend=/usr/libexec/cups/backend
cupsfilter=/usr/libexec/cups/filter
drv=/usr/share/cups/drv/hp
bin=/usr/bin
apparmor=/etc/apparmor.d
# Following values are determined at configure time and cannot be changed.
[configure]
network-build=no
libusb01-build=no
pp-build=no
gui-build=no
scanner-build=no
fax-build=no
dbus-build=no
cups11-build=no
doc-build=no
shadow-build=no
hpijs-install=no
foomatic-drv-install=yes
foomatic-ppd-install=no
foomatic-rip-hplip-install=no
hpcups-install=yes
cups-drv-install=yes
cups-ppd-install=yes
internal-tag=3.19.12
restricted-build=no
ui-toolkit=no
qt3=no
qt4=no
qt5=no
policy-kit=no
lite-build=no
udev_sysfs_rules=no
hpcups-only-build=no
hpijs-only-build=no
apparmor_build=no
class-driver=no


Current contents of '/var/lib/hp/hplip.state' file:
Plugins are not installed. Could not access file: No such file or directory

Current contents of '~/.hplip/hplip.conf' file:
warning: Could not access file: No such file or directory
 <Package-name>        <Package-Desc>      <Required/Optional> <Min-Version> <Installed-Version> <Status>   <Comment>

-------------------------
| External Dependencies |
-------------------------

 error: cups          CUPS - Common Unix Printing System                           REQUIRED        1.1             -               INCOMPAT   'CUPS may not be installed or not running'
 gs                   GhostScript - PostScript and PDF language interpreter and previewer REQUIRED        7.05            9.52            OK         -
 error: xsane         xsane - Graphical scanner frontend for SANE                  OPTIONAL        0.9             -               MISSING    'xsane needs to be installed'
 error: scanimage     scanimage - Shell scanning program                           OPTIONAL        1.0             -               MISSING    'scanimage needs to be installed'
 error: dbus          DBus - Message bus system                                    REQUIRED        -               1.12.16         MISSING    'DBUS may not be installed or not running'
 policykit            PolicyKit - Administrative policy framework                  OPTIONAL        -               0.116           OK         -
 network              network -wget                                                OPTIONAL        -               1.20.3          OK         -
 error: avahi-utils   avahi-utils                                                  OPTIONAL        -               -               MISSING    'avahi-utils needs to be installed'

------------------------
| General Dependencies |
------------------------

 error: libjpeg       libjpeg - JPEG library                                       REQUIRED        -               -               MISSING    'libjpeg needs to be installed'
 error: cups-devel    CUPS devel- Common Unix Printing System development files    REQUIRED        -               -               MISSING    'cups-devel needs to be installed'
 error: cups-image    CUPS image - CUPS image development files                    REQUIRED        -               -               MISSING    'cups-image needs to be installed'
 error: libpthread    libpthread - POSIX threads library                           REQUIRED        -               b'2.31'         MISSING    'libpthread needs to be installed'
 error: libusb        libusb - USB library                                         REQUIRED        -               1.0             MISSING    'libusb needs to be installed'
 error: sane          SANE - Scanning library                                      REQUIRED        -               -               MISSING    'sane needs to be installed'
 error: sane-devel    SANE - Scanning library development files                    REQUIRED        -               -               MISSING    'sane-devel needs to be installed'
 error: libnetsnmp-devel libnetsnmp-devel - SNMP networking library development files REQUIRED        5.0.9           -               MISSING    'libnetsnmp-devel needs to be installed'
 error: libcrypto     libcrypto - OpenSSL cryptographic library                    REQUIRED        -               1.1.1           MISSING    'libcrypto needs to be installed'
 python3X             Python 2.2 or greater - Python programming language          REQUIRED        2.2             3.8.2           OK         -
 error: python3-notify2 Python libnotify - Python bindings for the libnotify Desktop notifications OPTIONAL        -               -               MISSING    'python3-notify2 needs to be installed'
 error: python3-pyqt4-dbus PyQt 4 DBus - DBus Support for PyQt4                         OPTIONAL        4.0             -               MISSING    'python3-pyqt4-dbus needs to be installed'
 error: python3-pyqt4 PyQt 4- Qt interface for Python (for Qt version 4.x)         REQUIRED        4.0             -               MISSING    'python3-pyqt4 needs to be installed'
 error: python3-dbus  Python DBus - Python bindings for DBus                       REQUIRED        0.80.0          -               MISSING    'python3-dbus needs to be installed'
 python3-xml          Python XML libraries                                         REQUIRED        -               2.2.8           OK         -
 error: python3-devel Python devel - Python development files                      REQUIRED        2.2             3.8.2           MISSING    'python3-devel needs to be installed'
 error: python3-pil   PIL - Python Imaging Library (required for commandline scanning with hp-scan) OPTIONAL        -               -               MISSING    'python3-pil needs to be installed'
 error: python3-reportlab Reportlab - PDF library for Python                           OPTIONAL        2.0             -               MISSING    'python3-reportlab needs to be installed'

--------------
| COMPILEDEP |
--------------

 error: libtool       libtool - Library building support services                  REQUIRED        -               -               MISSING    'libtool needs to be installed'
 error: gcc           gcc - GNU Project C and C++ Compiler                         REQUIRED        -               -               MISSING    'gcc needs to be installed'
 error: make          make - GNU make utility to maintain groups of programs       REQUIRED        3.0             -               MISSING    'make needs to be installed'

---------------------
| Python Extentions |
---------------------

 cupsext              CUPS-Extension                                               REQUIRED        -               3.19.12         OK         -
 hpmudext             IO-Extension                                                 REQUIRED        -               3.19.12         OK         -

----------------------
| Scan Configuration |
----------------------

error: NOT FOUND OR FAILED TO LOAD! Please reinstall HPLIP and check for the proper installation of scanext.
 error: scanext       Scan-SANE-Extension                                          REQUIRED        -               3.19.12         MISSING    'scanext needs to be installed'

--------------------------
| DISCOVERED USB DEVICES |
--------------------------

  Device URI                                Model                  
  ----------------------------------------  -----------------------
  hp:/usb/hp_LaserJet_1320_series?serial=0  HP LaserJet 1320 series
  0XXXXXXXXXX                                                      

---------------------------------
| INSTALLED CUPS PRINTER QUEUES |
---------------------------------

 
HP_LaserJet_1320
----------------
Type: Unknown
Device URI: usb://HP/LaserJet%201320%20series?serial=00XXXXXXXXXX


--------------
| PERMISSION |
--------------

USB             None                           Required        -        -        OK       Node:'/dev/bus/usb/003/002' Perm:'  root  lp rw- rw- r--'
 
-----------
| SUMMARY |
-----------

Missing Required Dependencies
-----------------------------
error: 'cupsys' package is missing/incompatible 
error: 'cupsys-client' package is missing/incompatible 
error: 'libdbus-1-dev' package is missing/incompatible 
error: 'libjpeg-dev' package is missing/incompatible 
error: 'libcupsys2-dev' package is missing/incompatible 
error: 'cupsys-bsd' package is missing/incompatible 
error: 'libcupsimage2-dev' package is missing/incompatible 
error: 'libc6' package is missing/incompatible 
error: 'libusb-1.0-0-dev' package is missing/incompatible 
error: 'sane' package is missing/incompatible 
error: 'libsane-dev' package is missing/incompatible 
error: 'libsnmp9-dev' package is missing/incompatible 
error: 'libssl-dev' package is missing/incompatible 
error: 'libtool' package is missing/incompatible 
error: 'gcc' package is missing/incompatible 
error: 'g++' package is missing/incompatible 
error: 'make' package is missing/incompatible 

Missing Optional Dependencies
-----------------------------
error: 'xsane' package is missing/incompatible 
error: 'sane-utils' package is missing/incompatible 
error: 'avahi' package is missing/incompatible 

Total Errors: 25
Total Warnings: 1


Done.

 

 

and for print pdf file , run below commands , But print mistake content (bad format) :

 

root@STM32MP1:~# systemctl list-unit-files | grep cups
org.cups.cupsd.path                    enabled        
org.cups.cups-lpd@.service             static         
org.cups.cupsd.service                 enabled        
org.cups.cups-lpd.socket               enabled        
org.cups.cupsd.socket                  enabled        
root@STM32MP1:~# lpstat -r
scheduler is running
root@STM32MP1:~# lpinfo -v
network beh
[  702.899714] usblp0: removed
file cups-brf:/
[  702.957808] usblp 3-1:1.0: usblp0: USB Bidirectional printer dev 2 if 0 alt 1 proto 2 vid 0x03F0 pid 0x1D17
direct usb://HP/LaserJet%201320%20series?serial=00XXXXXXXXXX
network ipp
network https
network lpd
network socket
network http

network ipps
root@STM32MP1:~# 
root@STM32MP1:~# hp-setup
warning: python-dbus not installed.

HP Linux Imaging and Printing System (ver. 3.19.12)
Printer/Fax Setup Utility ver. 9.0

Copyright (c) 2001-18 HP Development Company, LP
This software comes with ABSOLUTELY NO WARRANTY.
This is free software, and you are welcome to distribute it
under certain conditions. See COPYING file for more details.

(Note: Defaults for each question are maked with a '*'. Press <enter> to accept the default.)


Using connection type: usb

 
Setting up device: hp:/usb/hp_LaserJet_1320_series?serial=00XXXXXXXXXX



---------------------
| PRINT QUEUE SETUP |
---------------------


Please enter a name for this print queue (m=use model name:'hp_LaserJet_1320'*, q=quit) ?m
Using queue name: hp_LaserJet_1320
Locating PPD file... Please wait.

Found PPD file: lsb/usr/cupsfilters/HP-Color_LaserJet_CM3530_MFP-PDF.ppd
Description: 

Note: The model number may vary slightly from the actual model number on the device.

Does this PPD file appear to be the correct one (y=yes*, n=no, q=quit) ? 
Enter a location description for this printer (q=quit) ?q
OK, done.
root@STM32MP1:~# lpadmin -p HP_LaserJet_1320 -E -v usb://HP/LaserJet%201320%20series?serial=00XXXXXXXXXX
root@STM32MP1:~# lpadmin -d HP_LaserJet_1320
root@STM32MP1:~# lpstat -p -d
printer HP_LaserJet_1320 is idle.  enabled since Fri Feb  7 19:37:54 2020
system default destination: HP_LaserJet_1320
root@STM32MP1:~# lp -d HP_LaserJet_1320 output.pdf
request id is HP_LaserJet_1320-21 (1 file(s))

 

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Jean-Marc B
ST Employee

Hi @macrobert 

The hplip package misses a dependency on the package python3-dbus. Since this post https://community.st.com/t5/stm32-mpus-products/stm32mp157-hplip-support/td-p/196923 , the package hplip is provided into the OpenSTLinux distribution with the missing dependency.

Could you make a try by adding python3-dbus into your image please?

Best regards

--JM

Hi @Jean-Marc B 

after :   apt-get install python3-dbus
"warning: python-dbus not installed " resolved but errors remained .

root@STM32MP1:~# hp-check
/usr/bin/hp-check:685: SyntaxWarning: "is not" with a literal. Did you mean "!="?
  if 'getfacl' not in g and '' is not g and 'file' not in g:
Saving output in log file: /home/root/hp-check.log

HP Linux Imaging and Printing System (ver. 3.19.12)
Dependency/Version Check Utility ver. 15.1

Copyright (c) 2001-18 HP Development Company, LP
This software comes with ABSOLUTELY NO WARRANTY.
This is free software, and you are welcome to distribute it
under certain conditions. See COPYING file for more details.

Note: hp-check can be run in three modes:
1. Compile-time check mode (-c or --compile): Use this mode before compiling the HPLIP supplied       
tarball (.tar.gz or .run2. Run-time check mode (-r or --run): Use this mode to determine if a distro supplied package (.deb,  
.rpm, etc) or an already built HPLIP supplied tarball has the proper dependencies installed to        
successfully run.                                                                                     
3. Both compile- and run-time check mode (-b or --both) (Default): This mode will check both of the   
above cases (both compile- and run-time dependencies).                                                

Check types:                                                                                          
a. EXTERNALDEP - External Dependencies                                                                
b. GENERALDEP - General Dependencies (required both at compile and run time)                          
c. COMPILEDEP - Compile time Dependencies                                                             
d. [All are run-time checks]                                                                          
PYEXT SCANCONF QUEUES PERMISSION                                                                      

Status Types:
    OK
    MISSING       - Missing Dependency or Permission or Plug-in
    INCOMPAT      - Incompatible dependency-version or Plugin-version

warning: st openstlinux - eglfs - (a yocto project based distro) distro is not found in AUTH_TYPES
warning: 50-3.1-snapshot-20231024 version is not supported. Using 50-6 versions dependencies to verify and install...

---------------
| SYSTEM INFO |
 Kernel: 5.4.31 #1 SMP PREEMPT Wed May 8 07:13:52 UTC 2024 GNU/Linux
 Host: STM32MP1
 Proc: 5.4.31 #1 SMP PREEMPT Wed May 8 07:13:52 UTC 2024 GNU/Linux
 Distribution: 50 3.1-snapshot-20231024
 Bitness: 32 bit


-----------------------
| HPLIP CONFIGURATION |
-----------------------

HPLIP-Version: HPLIP 3.19.12
HPLIP-Home: /usr/share/hplip
warning: HPLIP-Installation: Auto installation is not supported for 50 distro  3.1-snapshot-20231024 version 

Current contents of '/etc/hp/hplip.conf' file:
# hplip.conf.  Generated from hplip.conf.in by configure.

[hplip]
version=3.19.12

[dirs]
home=/usr/share/hplip
run=/var/run
ppd=/usr/share/ppd/HP
ppdbase=/usr/sre/doc/hplip-3.19.12
html=/usr/share/doc/hplip-3.19.12
icon=/usr/share/applications
cupsbackend=/usr/libexec/cups/backend
cupsfilter=/usr/libexec/cups/filtehare/cups/drv/hp
bin=/usr/bin
apparmor=/etc/apparmor.d
# Following values are determined at configure time and cannot be changed.
[configure]
network-build=no
libusb01-build=no
pp-build=no
gui-build=no
scanner-build=no
fax-build=no
dbus-build=no
cups11-build=no
doc-build=no
shadow-build=no
hpijs-install=no
foomatic-drv-install=yes
foomatic-ppd-install=no
foomatic-rip-hplip-install=no
hpcups-install=yes
cups-drv-install=yes
cups-ppd-install=yes
internal-tag=3.19.12
restricted-build=no
ui-toolkit=no
qt3=no
qt4=no
qt5=no
policy-kit=no
lite-build=no
udev_sysfs_rules=no
hpcups-only-build=no
hpijs-only-build=no
apparmor_build=no
class-driver=no


Current contents of '/var/lib/hp/hplip.state'le or directory

Current contents of '~/.hplip/hplip.conf' file:
warning: Could not access file: No such file or directory
 <Package-name>        <Package-Desc>      <Required/Optional> <Min-Version> <Installed-Version> <Status>   <Comment>

-------------------------
| External Dependencies |
-------------------------

 error: cups          CUPS - Common Unix Printing System                           REQUIRED        1.1             -               INCOMPAT   'CUPS may not be installed or not running'
 gs                   GhostScript - PostScript and PDF language interpreter and previewer REQUIRED        7.05            9.52            OK         -
 error: xsane         xsane - Graphical scanner frontend for SANE                  OPTIONAL        0.9             -               MISSING    'xsane needs to be installed'
 error: scanimage     scanimage - Shell scanning program                           OPTIONAL        1.0             -              'scanimage needs to be installed'
 error: dbus          DBus - Message bus system                                    REQU policykit            PolicyKit - Administrative policy framework                  OPTIONAL        -               0.116           OK         -
 network              network -wget                                                OPTIONAL        -               1.20.3          OK         -
 error: avahi-utils   avahi-utils                                                  OPTIONAL        -               -               MISSING    'avahi-utils needs to be installed'

------------------------
| General Dependencies |
------------------------

 error: libjpeg       libjpeg - JPEG library                                       REQUIRED        -               -               MISSING    'libjpeg needs to be installed'
 error: cups-devel    CUPS devel- Common Unix Printing System development files    REQUIRED        -               -               MISSING    'cups-devel needs to be instalage development files                    REQUIRED        -               -               MISSING    'cups-image needs to be installed'
 error: libpthread    libpthread - POSIX threads library                           REQUIRED        -               b'2.31'         MISSING    'libpthread needs to be installed'
 error: libusb        libusb - USB library                                         REQUIRED        -               1.0             MISSING    'libusb needs to be installed'
 error: sane          SANE - Scanning library                                      REQUIRED        -               -               MISSING    'sane needs to be installed'
 error: sane-devel    SANE - Scanning library development files                    REQUIRED        -               -               MISSING    'sane-devel needs to be installed'
 error: libnetsnmp-devel libnetsnmp-devel - SNMP networking library development files REQUIRED        5.0.9           -               MISSING    'libnetsnmp-devel needs to be installed'
 error: libcrypto     libcrypto - OpenSSL cryptographic library                    REQUIRED        -               1.1.1           MISSING    'libcrypto
 python3X             Python 2.2 or greater - Python programming language          REQUIRED        2.2             3.8.2        libnotify Desktop notifications OPTIONAL        -               pport for PyQt4                         OPTIONAL        4.0             -               MISSING    'python3-pyqt4-dbus needs to be installed'
 erro-pyqt4 PyQt 4- Qt interface for Python (for Qt version 4.x)         REQUIRED        4.0             -               MISSING    'python3-pyqt4 needs to be installed'
 python3-dbus                       REQUIRED        -               2.2.8           OK         -
 error: python3-devel Python devel - Python development files                      REQUIRED        2.2             3.8.2ython3-devel needs to be installed'
 error: python3-pil   PIL - Python Imaging Library (required for commandline scanning with hp-scan) OPTIONAL        -               -               MISSING    'python3-pil needs to be installed'
 error: python3-reportlab Reportlab - PDF library for Python                           OPTIONAL        2.0             -               MISSING    'python3-repo-----
| COMPILEDEP |
---------btool - Library building support services                  REQUIRED        -               -               MISSING    'libtool nlled'
 error: gcc           gcc - GNU Project C and C++ Compiler                         REQUIRED        -               -               MISSING    'gcc needs to be installed'
 error: make          make - GNU make utility to maintain groups of programs       REQUIRED        3.0             -  ds to be installed'

---------------------
| Python Extentions |
---------------------

 cupsext              CUPS-Extension                                                              REQUIRED        -               OK         -

----------------------
| Scan Configuration: NOT FOUND OR FAILED TO LOAD! Please reinstall HPLIP and check .
 error: scanext       Scan-SANE-Extension                                          REQUIRED        -               3.19.12         MISSING    'sc----------
| DISCOVERED USB DEVICES |
-----------------------  Device URI                                Model                  
  ----------------------------------------  ---------------=0  HP LaserJet 1320 series
  0XXXXXXXXXX                                                      

---------------------------------
| INSTALLED CUPS PRINTER QUEUES |
---------------------------------

 
HP_LaserJet_1320
----------------
Type: Unknown
Device URI: usb://HP/LaserJet%201320%20series?serial=00XXXXXXXXXX


--------------
| PERMISSION |
--------------

USB             None                           Required        -        -        OK       Node:'/dev/bus/usb/003/005' Perm:'  root  lp rw- rw- r--'
 
-----------
| SUMMARY |
-----------

Missing Required Dependencies
-----------------------------
error: 'cupsys' package is missing/incompatible 
error: 'cupsys-client' package is missing/incompatible 
error: 'libdbus-1-dev' package is missing/incompatible 
error: 'libjpeg-dev' package is missing/incompatible 
error: 'libcupsys2-dev' package is missing/incompatible 
error: 'cupsys-bsd' package is missing/incompatible 
error: 'libcupsimage2-dev' package is missing/incompatible 
e 'sane' package is missing/incompatible 
error: 'libsane-dev' package is missing/incompatible 
error: 'libsnmp9-dev' package is missing/incompatible 
error: 'libssl-dev' package is missing/incompatible 
error: 'libtool' package is missing/incompatible 
error: 'gcc' package is missing/incompatible 
error: 'g++' package is missing/incompatible 
error: 'make' package is missing/incompatible 

Missing Optional Dependencies
-----------------------------
error: 'xsane' package is missing/incompatible 
error: 'sane-utils' package is missing/incompatible 
error: 'avahi' package is missing/incompatible 

Total Errors: 24
Total Warnings: 1


Done.

 

macrobert
Associate II

hi  @Jean-Marc B 
Is there any support?

Hi @macrobert 

there are a lot of dependencies not met. Some of them are not provided by our package repository (*-dev packages for example).

I would suggest to work from a Distribution Package (see https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package) and install a local package repository (see https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution#How_to_activate_a_local_package_repository).

Then you will be able to install the missing packages from your own repository with the apt-get install command.

Best regards

--JM