STM32 MCUs
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

How to manage multiple EXTIs with the STM32Cube HAL

How to manage multiple EXTIs with the STM32Cube HAL1. Introduction It is very common to have multiple GPIOs used as External Interrupt (EXTI) sources in an embedded system. But how to manage them in an application code? This is exactly what is going ...

1847.png 1848.png 1849.png 1850.png

How to configure and use the PSSI on the STM32H7

How to configure and use the PSSI on the STM32H71. Introduction The PSSI which stands for Parallel synchronous slave interface and was introduced in our high performance STM32H7 family. The PSSI can be used as a fast interface between two STM32 micro...

1735.jpg 1736.png 1737.png 1738.png

How can I automate TraceX reads from STM32CubeIDE?

How can I automate TraceX reads from STM32CubeIDE?To make TraceX automatically fetch information, we can create a batchfile and run it with the debug session of the STM32CubeIDE Goal: Add TraceX support to STM32CubeIDE using X-CUBE-AZRTOS-H7 and make...

156.png 158.png 160.png 162.png

STM32H7 configuration tips and tricks

The STM32H7 products are part of the most powerful STM32 and bring many new features and capabilities. The drawback is the increase of the complexity of the system. Many resources are available on the ST community but also on the net to help you. The...

How to configure OctoSPI and QuadSPI with an STM32

1. OctoSPI You can find the detailed example with explanation inMOOC - STM32H72x/3x hands-on workshop - 6 Code execution from external FLASHIn this MOOC page you will find the link to the video and the full set of materials to download.Application No...

LauraCx by ST Employee
  • 3272 Views
  • 0 comments
  • 3 kudos

LoRa communication within STM32

What are the most important information to know about LoRa communication?What are the resources offered by ST and dedicated to the development of LoRa solutions?This FAQ concerns the LoRa communication, this tutorial contains the basic information to...

1311.png

What are Bluetooth Low Energy Packet Formats?

What are Bluetooth Low Energy Packet Formats?Summary This article details the Bluetooth LE packet formats for different applications from IoT to Automotive. 1.Link layer packet format  1.1 Bluetooth LE Protocol stack The Bluetooth LE protocol stack...

1616.png 1617.png 1618.png 1620.png
LauraCx by ST Employee
  • 5926 Views
  • 0 comments
  • 2 kudos

STM32 Arduino (STM32duino) tutorial

This FAQ concerns the STM32duino, after following this tutorial, it will be possible to get to know how to use STM32 Nucleo boards within the Arduino IDE and generate codes to run on them. In this article we use a STM32 Nucleo board and an ST MEMS sh...

1312.jpg 1313.jpg 1314.jpg 1315.jpg

STM32 QSPI interface address in Dual-Flash memory mode

Why does STM32 QSPI interface send addresses shifted right by 1bit in Dual-Flash memory mode?  The configured address in the QUADSPI_AR is divided by 2 (shifted right by 1bit) in DUAL bank mechanism, because each connected memory represents the half ...

704.png