User Activity

Continuation of Part 1,2,3.4. Teraterm Connection States The outputs to be presented are screen captures of both the client and server during the various states of the Whitelist demonstration process.  4.1 Initial Power Up Figure 3: Client Indication...
Summary This article represents Part 1 of a two-part series addressing methods in which to minimize the effects of external component noise and interference on the STM32WB and STM32WL series of devices. Part 1 will focus on the devices and circuits ...
Continuation of Part 1, Part 2  3.2 Client Configuration and Settings It is now necessary to open and edit the client application.  The following modifications are required to be implemented.Table 5 shows the modifications required to the SW 1 functi...
Continuation of previous parts3. Project Modifications The project code modifications for both the client and server are provided.  3.1 Client and Server Common Modifications: The key modifications common to both client and server are provided below....
Summary This article summarizes the procedure required to configure both Central and Peripheral devices, operating on individual STM32WB platforms for Whitelisting operation. A description of the Whitelisting operation within the context of Bluetoot...