cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-LRWAN2 - gateway firmware sources

lucasdietrich
Associate

 

Hello,

The firmware for the P-NUCLEO-LRWAN2 gateway is currently provided as a binary file named "st-nucleo-lora-gw-at-fw-v2.1.7-eu868-TTN.bin." I am very interested in obtaining access to the source code to develop a modified version of the firmware for personnal uses.

I understand that the P-NUCLEO-LRWAN2 kit is obsolete, but I continue to use the gateway as a packet forwarder for instrumentation and experimentation. Unfortunately, it does not support the latest version of the Semtech UDP protocol, which requires a TX_ACK to be sent after transmitting a packet (as specified here: https://github.com/Lora-net/packet_forwarder/blob/master/PROTOCOL.TXT). This limitation causes issues with multiple network servers. I would like to address this issue myself and make a few other minor modifications.

Could you please let me know if the source code is fully closed, or if there is a way to obtain it?

Best regards.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @lucasdietrich 

The gateway firmware binary is available upon request directly from STMicroelectronics. So, I suggest you contact directly one of our Sales and marketing teams.

Best regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Andrew Neil
Evangelist III

I think the source is 3rd-party (Rising HF?) - so you'd have to go to them ...

 

Hello Andrew,

I have already contacted RisingHF. They confirmed that while they designed the kit for ST, ST retains the copyright for the firmware.

Best regards.

Hello @lucasdietrich 

The gateway firmware binary is available upon request directly from STMicroelectronics. So, I suggest you contact directly one of our Sales and marketing teams.

Best regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.