2024-07-04 9:45 AM - edited 2024-07-04 9:46 AM
Hello,
The firmware for the P-NUCLEO-LRWAN2 gateway is currently provided as a binary file named "st-nucleo-lora-gw-at-fw-v2.1.7-eu868-TTN.bin." I am very interested in obtaining access to the source code to develop a modified version of the firmware for personnal uses.
I understand that the P-NUCLEO-LRWAN2 kit is obsolete, but I continue to use the gateway as a packet forwarder for instrumentation and experimentation. Unfortunately, it does not support the latest version of the Semtech UDP protocol, which requires a TX_ACK to be sent after transmitting a packet (as specified here: https://github.com/Lora-net/packet_forwarder/blob/master/PROTOCOL.TXT). This limitation causes issues with multiple network servers. I would like to address this issue myself and make a few other minor modifications.
Could you please let me know if the source code is fully closed, or if there is a way to obtain it?
Best regards.
Solved! Go to Solution.
2024-07-04 11:59 PM
Hello @lucasdietrich
The gateway firmware binary is available upon request directly from STMicroelectronics. So, I suggest you contact directly one of our Sales and marketing teams.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-04 10:46 AM
I think the source is 3rd-party (Rising HF?) - so you'd have to go to them ...
2024-07-04 1:03 PM
Hello Andrew,
I have already contacted RisingHF. They confirmed that while they designed the kit for ST, ST retains the copyright for the firmware.
Best regards.
2024-07-04 11:59 PM
Hello @lucasdietrich
The gateway firmware binary is available upon request directly from STMicroelectronics. So, I suggest you contact directly one of our Sales and marketing teams.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.