cancel
Showing results for 
Search instead for 
Did you mean: 

The setup instructions for the workshop seem to say you're supporting windows only - everything you specify is available on for mac and work fine - is there any problem participating if you're running on a mac?

RPoll.1
Associate
 
2 REPLIES 2
Radek RIPA
ST Employee

Hello,

For last hands-on we are using two batch files which will use third party tools(openssl, bytereverseutility, srecord). This I prepared only for windows.

But is possible to follow the hands-on without problems. Only the last step of encrypting of binary using batch file is not possible to repeat.

Best regards

Radek

RPoll.1
Associate

Thanks very much - I can run on a VM in that case.

...rob