Hello,For last hands-on we are using two batch files which will use third party tools(openssl, bytereverseutility, srecord). This I prepared only for windows. But is possible to follow the hands-on without problems. Only the last step of encrypting o...
Hello,I can confirm your findings. For both devices. Which have same error, where is not counted with situation that is additional content in shift register. If SPI IRQ is delayed the overrun is caused as result. Im reporting this to our SW team to f...
Posted on February 07, 2018 at 09:32
Hello,
Thank you for your report.
I can confirm the behavior.
When the project is created there are for some reason a virtual folders instead of real ones. This cause that the compilation will fail.
...
Posted on September 07, 2017 at 14:57
Hello,
you are right you are missing the CDC_GET_LINE_CODING and SET_LINE_CODING function.
The VCP still thinks that you are an COM port. For this PC sends the configuration and then reads it back.
I...