cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l496: Clocking timer using LSCO

HZaib.1
Associate III

Hi, I wanted to clock my timer output using LSE crystal, but unfortunately only tim2 is supported with this feature. 

But then I saw an option of LSCO as output in cubemx, this enables the pin on MCU and according to documentation this output LSE clock on that pin. So I was thinking about routing this signal to timer input as timer is going to be configured in ETR mode. So my question here is has anyone tried it and does it work ? is it even possible to route LSCO to multiple timer inputs ? 

 

I cant test it as I dont have a dev kit on my hand and only a custom board. 

4 REPLIES 4

What chip are you actually using?

stm32l496

So why have you tagged 7 other families too?

 

to reach every audience, as I guess this feature is also available in other series as well