2023-03-15 12:56 AM
*Using FP-AI-Vision1 Pack
import the binary webcam, the screen is black.
import the people detection binary, the screen is a mess.
No camera picture.
While import the Tutti Frutti demo, it can normally run.
Solved! Go to Solution.
2023-06-02 02:34 AM
Hello ,
The fix is available on GitHub :
In fact , LCD DSI MB1166-A9 delivered with latest version of STM32H747I-DISCO/ boards come based on LCD FGRIDA FRD400B25025-A-CTK instead of FRD397B25009-D-CTK.
Now the firmware is updated , you just need to enable the right hardware component as defined in stm32h747i_discovery_conf.h file and add the new component library (NT35510) in your project .
/* IMPORTANT: One of the following flags must be enabled in stm32h747i_discovery_conf.h file */
/* options in order to select the target daughter board revision connected on STM32H747I DISCOVERY : !!!!!!!!!! */
/* USE_LCD_CTRL_OTM8009A */ /* Applicable for all LCD daughter boards (MB1166) except for Rev -A09 */
/* USE_LCD_CTRL_NT35510 */ /* Applicable only for LCD daughter boards (MB1166) Rev -A09 */
2023-03-15 08:03 AM
Hello @Az.2 ,
Thank you for reporting the issue.
Which MB1166 Rev.A revision are you Using? A01, A03...?
You can find the MB1166 revision as shown in the below figure.
Thank you,
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-15 08:29 AM
Thanks for help! A03
2023-03-16 01:31 AM
Hello @Az.2 ,
Thank you.
I will check and I will get back to you as soon as possible.
Koauthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-21 01:31 AM
Hello @Az.2 ,
This issue is already reported in this post.
I confirm the issue on my side, it has been reported.
Internal ticket number: 147459 (This is an internal tracking number and is not accessible or usable by customers).
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-14 09:13 AM - edited 2023-11-20 09:12 AM
Hi, excuse me
How's the issue going?I'm using these binaries and all of them shows mess on the screen
2023-05-03 04:10 AM - edited 2023-11-20 09:13 AM
Hello @AZ.2
could you please give me the S/N (serial number) for your LCD , you can find how identify your SN on the picture below ,Thank you
2023-05-03 04:16 AM
I've commented in another questionFeed Detail (st.com)
The best comment is from me, I've uploaded some pictures about this issue.
(The default screen serial num is A225300780 with a QR code on right.
The new screen is A214500023 without QR code.)
2023-05-03 06:25 AM
Hello ,
Thank you.
I will check this S/N and I will get back to you ASAP
2023-06-02 02:34 AM
Hello ,
The fix is available on GitHub :
In fact , LCD DSI MB1166-A9 delivered with latest version of STM32H747I-DISCO/ boards come based on LCD FGRIDA FRD400B25025-A-CTK instead of FRD397B25009-D-CTK.
Now the firmware is updated , you just need to enable the right hardware component as defined in stm32h747i_discovery_conf.h file and add the new component library (NT35510) in your project .
/* IMPORTANT: One of the following flags must be enabled in stm32h747i_discovery_conf.h file */
/* options in order to select the target daughter board revision connected on STM32H747I DISCOVERY : !!!!!!!!!! */
/* USE_LCD_CTRL_OTM8009A */ /* Applicable for all LCD daughter boards (MB1166) except for Rev -A09 */
/* USE_LCD_CTRL_NT35510 */ /* Applicable only for LCD daughter boards (MB1166) Rev -A09 */