2023-03-06 6:03 AM
i just received my brand new stm32h747 discovery board, on power-up it does nothing just two LEDs light up, according to the user manual it should be preloaded with a demo.
I checked in cube prog and it reports as blank.
Is it possible that my device got damaged somehow or it is just not flashed?
aren't units tested before shipping out?
Is this a common thing? I don't remember ever receiving a discovery board blank
Solved! Go to Solution.
2023-05-01 12:00 AM - edited 2023-11-20 7:38 AM
Update: clicking the button on STM32 Cube Programmer that says "USB" and selecting "STLINK" on the pull-down menu enabled connection, resulting to the screen below, so I presume that if I can find the demo firmware it could be downloaded, right?
2023-05-01 10:13 AM
My statement above "the compiled demo can be found on the STM32H747I-DISCO product website in the subfolder STM32H747I-DISCO_demo/Binary" means:
In the meantime I have expressed the previous statement a little more comprehensibly and corrected it accordingly above, I would like to apologise very much for the problems of understanding.
2023-05-01 10:30 AM
Would you be able to tell me when the problem with the latest batch of screens will be resolved? I have purchased 20 of these for a demonstration and the original board works perfectly. The cloans unfortunately do not work due to incompatible screens. about 6 weeks on from reporting the error, I am hoping I do not need to return them all and re-write all the code onto a new board. So any update, no matter how small would be greatly appreciated. Thanks
2023-05-01 10:34 AM
Theoretically correct, but not quite sufficient, because an external flash must also be programmed, which must first be communicated to the STM32Cube programmer.
To make your work easier, however, you will find in the demo ZIP not only the HEX that contains the programme for the STM32H747 as well as for the external data flash, but also the appropriate BAT file for fully automated programming.
Since the BAT file is not encrypted, the command sequence can also be used for other operating systems if it is adapted accordingly.
Hope that helps?
Regards
/Peter
2023-05-03 1:59 AM
Hello Peter,
Thanks for your help. As mentionned in another post, I have also a Discovery Kit stm32h747i-disco (Coming from mouser without blister) which does nothing just two LEDs light up, One red on top and one green on back.
I read carefully all your recommendations. I get the en.STM32H747I-DISCO_demo. In Binary, I used the program_hexfile.bat file which looks to works well. I got the execution file with file boot and erase status and then, I got the loading progress bar. This progress bar disappeared at 92%. Nothing say, if the recording is right ?
Anyway, I was thing to have something on the screen but it remain black.
I understood, program_hexfile.bat program both internal Flash and external QSPI memory. Is that right ?
In the readme,txt, they talk of the file "STM32Cube_Demo-STM32H747I-DISCO-VX.Y.Z_FULL.hex" when in binary the file is STM32Cube_Demo-STM32H747I-DISCO-V1.0.0_FULL,hex. Is that an issue.
I also programm a flash 32 Gb, as mentionned in the text. I Checked images,sounds and videos on the computer. Everything looks Good. Anyway, I imagine, even without flash, the demo programm should show at least a menu. Is that right ?
What is wrong ?
Best Regards
Robert
2023-05-05 7:19 AM
Hello,
Some news about this issus not yet solve for me.
I used the program_hexfile.bat file again. I got the loading progress bar. This progress bar disappeared at 96%. The screen was still black after completion.
But, at that time, I restart my computer for another reason, the disco 747 board beeing still connected. And suddenly, the demo appeared. It was working well.
Then, I disconnect the board but the screen remain black. I try to restart my computer, but the sreen is still black
Best Regards
Robert
2023-05-05 4:38 PM
> In the readme,txt, they talk of the file "STM32Cube_Demo-STM32H747I-DISCO-VX.Y.Z_FULL.hex" when in binary the file is STM32Cube_Demo-STM32H747I-DISCO-V1.0.0_FULL,hex. Is that an issue.
Seriously? No capabilities of figuring out on your own what those letters with dots might mean?
2023-05-05 11:22 PM
Seriously, you are right. So, I assume, it's probably not a version issue.
But, my nice new DISCO has not yet a Demo.
Any ideas ?
Best regards
2023-05-06 12:02 AM - edited 2023-11-20 7:38 AM
As you are having trouble flashing this you could install TouchGFX, the demo is contained in there, create a project in TouchGFX using the board and the demo and then you can flash it from within TouchGFX, it will handle everything for you.
2023-05-06 12:55 AM
Yes, the TouchGFX demos worked to my surprise. Once flashed, I found my old code written in CubeIDE could then be flashed as normal. If I flashed directly on a new board without first loading something (even a blank screen from TouchGFX), my CubeIDE code crashed the board. Not sure if that helps anyone, but just my experience yesterday.