Dear Help, I ran into a series of anomalies while following TouchGFX tutorial on Win10, resulting in code not able to run in Simulator and download failed in Programmer. Here are the steps and results:1. Using TouchGFX 4.21 and following Tutorial...
Hi, Chief, Thanks for the clarification. Yes, I found it very easy to start with TouchGFX to create the GUI on the -DISCO or DK boards with built-in displays also. My struggle was more with adding the additional controls and communication after...
Hi, I tried to follow several STmicro TouchGFX tutorial on youtube, which all started straight from TouchGFX Designer, create the code, and then add backend and interactions in CubeIDE. So am I correct that I should actually start from CubeMX to ...
Regarding the Core locked issue, I have since successfully downloaded other .elf codes again onto the stm32h7b3i-DK board, so the issue is only with the particular .elf file created with GFX code (attached).Benjamin
Thank you, Peter -- Yes, it helped. Thanks for fixing the link to the demo page also. Of course if I had read your instructions more carefully before clicking everywhere at random I'd have found the demos earlier ;-).Strangely, though, the demos (bot...
Update: clicking the button on STM32 Cube Programmer that says "USB" and selecting "STLINK" on the pull-down menu enabled connection, resulting to the screen below, so I presume that if I can find the demo firmware it could be downloaded, right?