cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 execute code in parallel FLASH

regjoe
Associate II

Hello,

I want to execute code located in external 16bit NOR FLASH e.g. on a STM32H7x3 evaluation board.

I can run the NOR FLASH demo (erase, write, read flash) successfully but have no clue how to create and flash code.

After googling 2 days I found plenty of examples for xSPI but none seems to suit this kind of flash type.

Can somebody point me into the right direction e.g. how to configure the linker script and flash the code using the debugger or Cube Programmer. Any example code or ANs?

Thank you

5 REPLIES 5
SofLit
ST Employee

Hello,

There is no direct example that provides an execution from External paralel NOR Flash.

As said in the previous thread, the AN4891 "STM32H72x, STM32H73x, and single-core STM32H74x/75x
system architecture and performance" with the package X-CUBE-PERF-H7 could help you to do what you are looking for and inspire from the execution from QSPI Flash.

What important is to configure the NOR flash in the system_stm32h7xx.c as done for QSPI memory in X-CUBE-PERF-H7. You need to find the Flash loader of that Flash memory and add it in the IDE. Otherwise you will use STM32CubeProgrammer and add that flash from External Flash loader and upload the .hex file generated from the IDE.

For the linker file you need to refer to the QSPI example scatter file: 8-M7-QSPI-Single_rwDTCM.sct for KEIL under Projects\STM32H743I_EVAL\stm32h7x3_cpu_perf\MDK-ARM\scatter_files

For IAR: C:\Users\sofiene\Downloads\en.x-cube-perf-h7\STM32CubeExpansion_Performance_H7_V1.0.0\Projects\STM32H743I_EVAL\stm32h7x3_cpu_perf\EWARM\icf_files

And for system workbench Projects\STM32H743I_EVAL\stm32h7x3_cpu_perf\SW4STM32\ where .ld file are located in the different project folders.

Hope it helps.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello SofLit,

in the eval board schematics of the STM32H7x3 Eval board in rev B and E are PC28F123M29EWLA and MT28EW128ABA1LPC-0SIT NOR FLASH, but the Cube Programmer seems to support M29W128GL only.

The M29W128GL seems to be out of production. I found a AN regarding writing external flash loaders and sources of the M29W128GL can be found on GITHUB, so it should be possible to use recent chips. Hope this task is not too complicated and time consuming. I will run into the same problem for QSPI FLASH later.

BTW: Beside ST there is another interesting project on GITHUB with lots of ports to the latest Q/OSPI flashes, but most of them seem to be in pending status.

I'll dive into the code you mentioned. I probably need additional information how to flash external memory using Cube IDE and where to find suitable flash loaders.

Best regards

 

 

Hello,

If possible to give a try by uploading the binary demo of that board using CubeProgrammer with the M29Wxxx flash loader:  https://www.st.com/resource/en/compiled_demos/stm32h743i-eval_demo.zip

If it doesn't work, I will ask internally if there is a Flash loader for MT28EW128 available.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Sorry, it seems  that the demo doesn't use External Flash NOR on FMC. It uses only QSPI Flash NOR.

So I will ask internally for MT28EW128 Flash loader availability.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I think the flash on my STM32H753_EVAL2 board rev E has a MICRON logo printed on top.

The Cube Programmer contains an external loader for the M29W128GL for the STM32H743 evaluation board.

So hopefully, this might work. I'll check than as soon as I get the demo compiled.

Any additional information from your team is welcome.