cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8T6 - Stop and start timers timebase inside an interruption

EMart.10
Associate II

Hi! I'm working in an application where I want to start a series of ADC conversions every 10 seconds, take a hundred samples and stop the conversions. The way I thought of it is to use a timer (timer 1 in my case) to measure the 10 seconds and use another timer (timer 3) to trigger the ADC conversions. Once the 100 conversions are made, the timer 3 stops until the timer 1 counts to 10 seconds again.
The problem that I have is that the timer 3 does the cycle only one time and after disabling the time base inside the ADC callback function I can't start it again from the TIM1 callback function. This works fine only if I don't use HAL_TIM_Base_Stop(&htim3).
Am I doing something wrong or this method is not possible?

 

 

 

 

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_9); HAL_TIM_Base_Start(&htim3); } void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 1); counter++; sumVoltage += adcResults[0]; sumBattCurrent += adcResults[1]; if (counter == 100){ voltage = sumVoltage / 100.0 * (3.285 / 4095.0); battCurrent = ((sumBattCurrent / 100.0) - 3080.0) / 61.0; counter = 0; sumVoltage = 0; sumBattCurrent = 0; HAL_TIM_Base_Stop(&htim3); } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 0); } static void MX_ADC1_Init(void) { ADC_ChannelConfTypeDef sConfig = {0}; hadc1.Instance = ADC1; hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T3_TRGO; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 3; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_7CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } sConfig.Channel = ADC_CHANNEL_8; sConfig.Rank = ADC_REGULAR_RANK_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } sConfig.Channel = ADC_CHANNEL_TEMPSENSOR; sConfig.Rank = ADC_REGULAR_RANK_3; sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } } static void MX_TIM1_Init(void) { TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; htim1.Instance = TIM1; htim1.Init.Prescaler = 1835; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 65358; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim1) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); } } static void MX_TIM3_Init(void) { TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; htim3.Instance = TIM3; htim3.Init.Prescaler = 0; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 419; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) { Error_Handler(); } }
View more

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

> I can't start it again

What is it that you can't start? TIM3 or the ADC conversions? What are exactly the symptoms? What are TIM3 registers content, mainly TIM3_CR1.CEN?

JW

View solution in original post

2 REPLIES 2

> I can't start it again

What is it that you can't start? TIM3 or the ADC conversions? What are exactly the symptoms? What are TIM3 registers content, mainly TIM3_CR1.CEN?

JW

Thanks! I'm new to this and don't know much about the registers and low level stuff, with your reply I managed to start the timer 3 and trigger the conversions again after changing the CEN bit in CR1 with TIM3 -> CR1 |= (1 << 0).