2024-09-27 9:31 AM
I am looking to stream audio over an ethernet connection to a cellular hot spot. This will be low latency. Can someone tell me what STM32 firmware library I should use and if this is an appropriate hardware for that task?
Thanks
2024-09-28 4:58 AM - edited 2024-09-28 4:58 AM
Define "audio": how many channels? bit rate? bit depth?
Define "low latency".
When you say "ethernet", is that purely at the physical layer, or do you also need to be IP-based?
Especially with IP, it is a non-trivial exercise - doubly so with wireless links.
https://en.wikipedia.org/wiki/Audio_over_Ethernet
2024-09-28 2:14 PM - edited 2024-09-29 2:45 PM
Hello Andrew.
Great questions!
This will be up to about 10kHz 12kHz.
Low latency will be sub second.
IP-based.
Right now my vision (and please feel free to jump in here).
I have a NUCLEO-H723ZG on the way. I am looking at the X-CUBE-OPUS and X-CUBE-ETHERNET libraries to integrate. I 'hope' I can take A/D samples, create PCM for the OPUS and send to the ETHERNET library. Initially I want to get the pieces in place and do a proof of concept. On the final solution I am still out on the fence as whether to use UDP/Multicasting vs TCP to a website and hosting....I guess it comes down to reliability vs latency in that sense.
Thoughts?
Steve
2024-09-30 1:39 AM
@SWenn.1 wrote:This will be up to about 10kHz 12kHz.
Is that your sample rate?
What bit-depth?
Mono or stereo?
@SWenn.1 wrote:Low latency will be sub second.
eg, 950ms would be OK ?
Another issue to consider on IP networks is the allowable "jitter" on that ...
2024-09-30 5:17 AM
Sample rate (whatever OPUS allows)...24 or 48khz
bit depth....16 if possible, if not 12 and padded for PCM
mono....
if 950 is the best I can get then so be it...(if you have another lower latency path in the confines of that nucleo I mentioned I would love to hear it)
2024-09-30 6:01 AM
I'm doing that with the H723 / H733 / H735.
8 audio channels (I2S from the 2 SAIs) at 32 bit / 200 kHz (51.2 Mbit/s) via DMA to internal SRAM buffers to HyperRAM via DMA to ETH via TCP to PC host.
I use lwIP (some minor parts tuned a little) and self-made ETH-driver, no OS.
CPU at 400 MHz, no audio processing, CPU sleeping about 50%.
Works like a charm.
If you have a client that's taking data quickly and reliably (so just do not plug into "a network" but directly to host) you probably don't need extra RAM, and latency will be about 2 packet times (guessing: < 5 ms).
So how many audio channels do you have, just this one?
Anyway, at that sampling rate it shouldn't be a problem - BUT it will be lots of work.
Spoiler: CubeMX, and even many HAL functions will not do all the work for you.
In all of my "signal path" relevant code there's only HAL_GetTick() left from HAL. :D
2024-09-30 6:19 AM - edited 2024-09-30 6:42 AM
Just one audio channel. I too was hoping to avoid OS. That is really low latency! Can you explain the
" (so just do not plug into "a network" but directly to host)"....
My vision would be to send to a IP address of at say AWS and users could stream off of that...
2024-09-30 8:09 AM
> My vision would be to send to a IP address of at say AWS and users could stream off of that...
Live streaming to or from AWS? Anyway, I have no idea about that.
Sometimes Windows 10 alone has other stuff in mind, and the more nodes in the network, the more your latency goes up - and more than the inbuilt RAM might be needed (prolly not with 1 channel at 16b/48k).
So, my short latency is in a super small network: STM32 - PoE switch - PC.
I have seen latency go up in our company office network, depending on the traffic.
I have tweaked lwIP PCBs by adding DiffServ / QoS priorities, but I have no idea if that actually helped.
There's some more testing to do on my side...
2024-09-30 9:11 AM - edited 2024-09-30 9:14 AM
Thanks so much for the advice! One more quick question.....Do you know if / where there is an AAC codec ST library?
2024-10-01 4:58 AM
Sorry, I don't.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.