2024-08-12 03:12 AM - edited 2024-08-12 04:14 AM
Hi everyone,
I use the IS25LX064 OctoSPI Flash memory with the STM32H573 and after configuring the OctoSPI flash i can read the device Id of the flash successfully. But when i change the configuration of the Volatile configuration register by setting the dummy cycles (see function OSPI_DummyCycles in the code below) there is no change in the register. When i read the register after setting the dummy cycle i get 0xFF and so the change has no effect.
Does anyone know what could be the problem did i omit something in the configuration?
The gpio config is fine because i can read the device id . Also if i try to write to a reserved address of the volatile configuration register and then read the flag status register, i see that the error bit in the status register is set which is exepected. But writing to the dummy cycle address of the volatile config register has no effect and no error is reported in flag status register.
@AME MCU Support Center BB, @Tesla DeLorean, @Amel NASRI, @MNapi do you have any idea?
Datasheet of the controller
https://www.issi.com/WW/pdf/25LX-WX032-064.pdf
I use the following code to set the dummy cycles
static void MX_OCTOSPI1_Init(void) {
/* USER CODE BEGIN OCTOSPI1_Init 0 */
/* USER CODE END OCTOSPI1_Init 0 */
/* USER CODE BEGIN OCTOSPI1_Init 1 */
/* USER CODE END OCTOSPI1_Init 1 */
/* OCTOSPI1 parameter configuration*/
hospi1.Instance = OCTOSPI1;
hospi1.Init.FifoThresholdByte = 1;
hospi1.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
hospi1.Init.MemoryType = HAL_XSPI_MEMTYPE_MICRON;
hospi1.Init.MemorySize = HAL_XSPI_SIZE_8MB;
hospi1.Init.ChipSelectHighTimeCycle = 2;
hospi1.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
hospi1.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
hospi1.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
hospi1.Init.ClockPrescaler = 3;
hospi1.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
hospi1.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_ENABLE;
hospi1.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
hospi1.Init.DelayBlockBypass = HAL_XSPI_DELAY_BLOCK_BYPASS;
hospi1.Init.Refresh = 0;
if (HAL_XSPI_Init(&hospi1) != HAL_OK) {
Error_Handler();
}
/* USER CODE BEGIN OCTOSPI1_Init 2 */
/* USER CODE END OCTOSPI1_Init 2 */
}
static void ReadId(XSPI_HandleTypeDef *hospi) {
XSPI_RegularCmdTypeDef sCommand = { 0 };
uint8_t deviceId[20];
sCommand.OperationType = HAL_XSPI_OPTYPE_COMMON_CFG;
sCommand.Instruction = 0x9E; /*----- read device id command ------*/
sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_1_LINE;
sCommand.InstructionWidth = HAL_XSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDTRMode = HAL_XSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressMode = HAL_XSPI_ADDRESS_NONE;
sCommand.AlternateBytesMode = HAL_XSPI_ALT_BYTES_NONE;
sCommand.DataMode = HAL_XSPI_DATA_1_LINE;
sCommand.DataDTRMode = HAL_XSPI_DATA_DTR_DISABLE;
sCommand.DataLength = 20;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_XSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_XSPI_SIOO_INST_EVERY_CMD;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
if (HAL_XSPI_Receive(hospi, deviceId, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
}
static void WriteEnable(XSPI_HandleTypeDef *hospi) {
XSPI_RegularCmdTypeDef sCommand = { 0 };
XSPI_AutoPollingTypeDef sConfig = { 0 };
/* Enable write operations ------------------------------------------ */
sCommand.OperationType = HAL_XSPI_OPTYPE_COMMON_CFG;
sCommand.Instruction = 0x06; /*----- write enable command ---*/
sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_1_LINE;
sCommand.InstructionWidth = HAL_XSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDTRMode = HAL_XSPI_INSTRUCTION_DTR_DISABLE;
sCommand.AddressMode = HAL_XSPI_ADDRESS_NONE;
sCommand.AlternateBytesMode = HAL_XSPI_ALT_BYTES_NONE;
sCommand.DataMode = HAL_XSPI_DATA_NONE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_XSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_XSPI_SIOO_INST_EVERY_CMD;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
/* Configure automatic polling mode to wait for write enabling ---- */
sCommand.Instruction = 0x05; /*---- read status register command ----*/
sCommand.DataMode = HAL_XSPI_DATA_1_LINE;
sCommand.DataDTRMode = HAL_XSPI_DATA_DTR_DISABLE;
sCommand.DataLength = 1;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
sConfig.MatchValue = 0x02; /*------- write enable value ---*/
sConfig.MatchMask = 0x02; /*--------write enable match-----*/
sConfig.MatchMode = HAL_XSPI_MATCH_MODE_AND;
sConfig.IntervalTime = AUTO_POLLING_INTERVAL;
sConfig.AutomaticStop = HAL_XSPI_AUTOMATIC_STOP_ENABLE;
if (HAL_XSPI_AutoPolling(hospi, &sConfig, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
}
static void OSPI_DummyCycles(XSPI_HandleTypeDef *hospi) {
XSPI_RegularCmdTypeDef sCommand = { 0 };
XSPI_AutoPollingTypeDef sConfig = { 0 };
uint8_t reg;
/* Enable write operations ---------------------------------------- */
WriteEnable(hospi);
sCommand.OperationType = HAL_XSPI_OPTYPE_COMMON_CFG;
sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_1_LINE;
sCommand.InstructionWidth = HAL_XSPI_INSTRUCTION_8_BITS;
sCommand.InstructionDTRMode = HAL_XSPI_INSTRUCTION_DTR_DISABLE;
sCommand.Instruction = 0x81; /*----- write volatile config register command---*/
sCommand.Address = 0x00000001;
sCommand.AddressMode = HAL_XSPI_ADDRESS_1_LINE;
sCommand.AddressWidth = HAL_XSPI_ADDRESS_32_BITS;
sCommand.AddressDTRMode = HAL_XSPI_ADDRESS_DTR_DISABLE;
sCommand.AlternateBytesMode = HAL_XSPI_ALT_BYTES_NONE;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_XSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_XSPI_SIOO_INST_EVERY_CMD;
sCommand.DataMode = HAL_XSPI_DATA_1_LINE;
sCommand.DataDTRMode = HAL_XSPI_DATA_DTR_DISABLE;
sCommand.DataLength = 1;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
reg = 0x06;
if (HAL_XSPI_Transmit(hospi, ®, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
/* Wait that the memory is ready ---------------------------------- */
sCommand.Instruction = 0x05; /*------- read status register command-------*/
sCommand.AddressMode = HAL_XSPI_ADDRESS_NONE;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
sConfig.MatchValue = 0x00;
sConfig.MatchMask = 0x01;
sConfig.MatchMode = HAL_XSPI_MATCH_MODE_AND;
sConfig.IntervalTime = AUTO_POLLING_INTERVAL;
sConfig.AutomaticStop = HAL_XSPI_AUTOMATIC_STOP_ENABLE;
if (HAL_XSPI_AutoPolling(hospi, &sConfig, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
/* ensure dummy cycle is set correctly */
sCommand.Instruction = 0x85; /*---- read volatile configuration register cmd----*/
sCommand.Address = 0x00000001;
sCommand.AddressMode = HAL_XSPI_ADDRESS_1_LINE;
if (HAL_XSPI_Command(hospi, &sCommand, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
uint8_t dummyCycles = 0;
if (HAL_XSPI_Receive(hospi, &dummyCycles, HAL_XSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK) {
Error_Handler();
}
}