2021-03-17 03:34 PM
Hello,
my problem is that i can't get access to the ADC12_CCR register. I activated the corresponding Clock in the RCC_AHB2ENR register. In addition I compare the addresses of the register from the library with the data of the reference manual, they are the same. I tried the same with the ADC345_CCR register, that access succeeded.
My minimal code is very simple without HAL or LL Library, so it's very clearly to understand.
PS: I also tried it with the HAL library, but the HAL Library also don't get access to this register.
#include "stm32g473xx.h"
void main(void)
{
RCC->AHB2ENR|=RCC_AHB2ENR_ADC12EN;
ADC12_COMMON->CCR=0x1C0000;
}
This CODE above don't work.
But the following code below is working...
#include "stm32g473xx.h"
void main(void)
{
RCC->AHB2ENR|=RCC_AHB2ENR_ADC345EN;
ADC345_COMMON->CCR=0x1C0000;
}
I don't no, it's a mysterium. I don't found a reason for a defect in the errata sheet.
Do i have miss some important information from the reference manual? Maybe is the address of the ADC12_CCR register (0x50000208) wrong?
Is there some clock I have to activate in addition?
On further try was with direct addressing of the register
#include "stm32g473xx.h"
void main(void)
{
RCC->AHB2ENR|=RCC_AHB2ENR_ADC12EN;
*((uint32_t*)0x50000208)=0x1C0000;
}
Solved! Go to Solution.
2021-03-19 07:58 AM
Ok, i find the fault. The address in the STM32G473xx_Peripherals.xml line was wrong.
And with direct addressing in my last minimal code, i also use the wrong address.
in this file #include "stm32g473xx.h" the address is correct and equal to the information given in the Reference Manual.
The .xml File which is used by the debugger from CrossStudio located in C:\Users\"your username"\AppData\Local\Rowley Associates Limited\CrossWorks for ARM\v4\packages\targets\STM32\include\STM32G473xx_Peripherals.xml has the wrong address. I update the address see below and now it works!
Line9728 <RegisterGroup name="ADC12_Common" start="0x50000200" description="Analog-to-Digital Converter"> is wrong
Line9728 <RegisterGroup name="ADC12_Common" start="0x50000300" description="Analog-to-Digital Converter"> is correct
2021-03-19 07:58 AM
Ok, i find the fault. The address in the STM32G473xx_Peripherals.xml line was wrong.
And with direct addressing in my last minimal code, i also use the wrong address.
in this file #include "stm32g473xx.h" the address is correct and equal to the information given in the Reference Manual.
The .xml File which is used by the debugger from CrossStudio located in C:\Users\"your username"\AppData\Local\Rowley Associates Limited\CrossWorks for ARM\v4\packages\targets\STM32\include\STM32G473xx_Peripherals.xml has the wrong address. I update the address see below and now it works!
Line9728 <RegisterGroup name="ADC12_Common" start="0x50000200" description="Analog-to-Digital Converter"> is wrong
Line9728 <RegisterGroup name="ADC12_Common" start="0x50000300" description="Analog-to-Digital Converter"> is correct
2021-03-24 11:50 AM
Thanks for sharing the solution.
You may perhaps want to let Rowley know, too.
JW
2021-03-26 11:31 AM
Hello @SMein.1 and welcome to the STM32 Community
Thanks for bringing this error to our attention.
I have passed this along to our development team for fix.
Imen