2021-03-18 2:00 AM
Hello , i would like to receive data via SPI . i tried to use getting data from AD7606 via HAL_SPI_Receive_dma , but i always failed. i do not know which step i miss or wrong . Could you give me hint or solution? Thanks for very much .
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_TIM7_Init();
MX_USART2_UART_Init();
/* Init scheduler */
osKernelInitialize();
/*handle */
SendTaskHandle = osThreadNew(SendTaskFun, NULL, &SendTask_attributes);
ReceiveTaskHandle = osThreadNew(ReceiveTaskFun, NULL, &ReceiveTask_attributes);
osKernelStart();
while (1) {
}
}
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
/* DMA2_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
/* DMA2_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
}
** Note
DMA2_Stream0 - > SPI1 Receive
DMA2_Stream3 - > SPI1 Transmit
DMA1_Stream4 - > SPI2 Transmit
void ReceiveTaskFun(void *argument)
{
uint8_t receive_buffer[256] ;
for (;;) {
//-- Enable CS
HAL_GPIO_WritePin(GPIO_A, GPIO_PIN_7, 0); //-- cs=0 active low
//- - SPI2_DMA_receive
...... (Here is for receive data from AD7606 )
HAL_SPI_Receive_DMA(&hspi1, receive_buffer, 8);
}
// From stm32f4XX_it.c
void DMA2_Stream0_IRQHandler(void)
{
/* USER CODE BEGIN DMA2_Stream0_IRQn 0 */
/* USER CODE END DMA2_Stream0_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_spi1_rx);
/* USER CODE BEGIN DMA2_Stream0_IRQn 1 */
DMA2->LISR |= 1<< 26;
/* USER CODE END DMA2_Stream0_IRQn 1 */
}
//From main.c function
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
if (hspi->Instance == SPI1){
HAL_GPIO_WritePin(GPIO_A, GPIO_PIN_7, 1); //-- cs=1 deactive
}
}
There is my code , I abbreviated the code. If some important codes that i did not paste on it , please tell me .
i refer DMA controller manual and stm32 f407 reference manual
Then , I set TCIF3(bit 27 ) to 1 after HAL_SPI_RxCpltCallback . But It worked only one time, the second dma receive did not perform. Did i miss any information about SPI_DMA? :\
2021-03-18 4:01 PM
IMO Cube/HAL clears the DMA flags for you.
> void ReceiveTaskFun(void *argument)
> {
> uint8_t receive_buffer[256] ;
You can't DMA into a local variable.
JW
2021-03-18 11:13 PM
Thanks your suggestion . i changed receive_buffer[256] to global variable . Then i fixed my code ,and dma work!
But there are some problems that I always received same data . As if i didn't receive any new data.
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hspi->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PB5 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* SPI1 DMA Init */
/* SPI1_RX Init */
hdma_spi1_rx.Instance = DMA2_Stream0;
hdma_spi1_rx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_rx.Init.Mode = DMA_NORMAL;
hdma_spi1_rx.Init.Priority = DMA_PRIORITY_HIGH;
hdma_spi1_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi1_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi1_rx);
/* SPI1_TX Init */
hdma_spi1_tx.Instance = DMA2_Stream3;
hdma_spi1_tx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi1_tx.Init.Mode = DMA_NORMAL;
hdma_spi1_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi1_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi1_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hspi,hdmatx,hdma_spi1_tx);
/* SPI1 interrupt Init */
HAL_NVIC_SetPriority(SPI1_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI1_Init();
MX_SPI2_Init();
MX_TIM7_Init();
MX_USART2_UART_Init();
uint8_t receive_buffer[256] ;
/* Init scheduler */
osKernelInitialize();
/*handle */
SendTaskHandle = osThreadNew(SendTaskFun, NULL, &SendTask_attributes);
ReceiveTaskHandle = osThreadNew(ReceiveTaskFun, NULL, &ReceiveTask_attributes);
osKernelStart();
while (1) {
}
}
static void MX_SPI1_Init(void)
{
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
/* DMA2_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
/* DMA2_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
}
** Note
DMA2_Stream0 - > SPI1 Receive
DMA2_Stream3 - > SPI1 Transmit
DMA1_Stream4 - > SPI2 Transmit
void ReceiveTaskFun(void *argument)
{
for (;;) {
//-- SPI1 callback
HAL_SPI_RxCpltCallback(&hspi1);
HAL_GPIO_WritePin(GPIO_A, GPIO_PIN_7, 1); //-- cs=1 deactive
}
// From stm32f4XX_it.c
void DMA2_Stream0_IRQHandler(void)
{
HAL_DMA_IRQHandler(&hdma_spi1_rx);
}
void DMA2_Stream3_IRQHandler(void)
{
HAL_DMA_IRQHandler(&hdma_spi1_tx);
}
//From main.c function
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
if (hspi->Instance == SPI1){
//-- Enable CS
HAL_GPIO_WritePin(GPIO_A, GPIO_PIN_7, 0); //-- cs=0 active low
//- - SPI2_DMA_receive
...... (Here is for receive data from AD7606 )
HAL_SPI_Receive_DMA(&hspi1, receive_buffer, 8);
}
}
2021-03-19 1:50 AM
I don't use Cube/HAL so can't help directly.
Try to clear the buffer between successive reception sessions, that would reveal if it really does not work.
Try to read out the SPI and DMA registers content before the "working" and "non-working" session and compare.
JW