Skip to main content
Associate II
March 11, 2025
Question

STM32wb55 does not show connected even if connected to the phone

  • March 11, 2025
  • 2 replies
  • 514 views

 

I have my device that is working on FreeRTOS. The main issue is that when I connect my device to an app (a custom or the ST BLE toolbox), I kill the app. If I relaunch the app, the device is not shown.

To check why it causes this issue, I check if my device is connected to the phone, for example, to try to relaunch the advertising.

But then I saw that my device stayed at BLE APP_BLE_FAST_ADV even if I was connected.

I also checked at two places if I am connected.
in custom_app.c in this function :

 
void Custom_APP_Notification(Custom_App_ConnHandle_Not_evt_t* pNotification)
{
 /* USER CODE BEGIN CUSTOM_APP_Notification_1 */

 /* USER CODE END CUSTOM_APP_Notification_1 */

 switch (pNotification->Custom_Evt_Opcode)
 {
 /* USER CODE BEGIN CUSTOM_APP_Notification_Custom_Evt_Opcode */

 /* USER CODE END P2PS_CUSTOM_Notification_Custom_Evt_Opcode */
 case CUSTOM_CONN_HANDLE_EVT:
 /* USER CODE BEGIN CUSTOM_CONN_HANDLE_EVT */

 /* USER CODE END CUSTOM_CONN_HANDLE_EVT */
 break;

 case CUSTOM_DISCON_HANDLE_EVT:
 /* USER CODE BEGIN CUSTOM_DISCON_HANDLE_EVT */

 /* USER CODE END CUSTOM_DISCON_HANDLE_EVT */
 break;

and in app_ble.c in this function :

 

SVCCTL_UserEvtFlowStatus_t SVCCTL_App_Notification(void* p_Pckt)
{

 p_event_pckt = (hci_event_pckt*)((hci_uart_pckt*)p_Pckt)->data;

 switch (p_event_pckt->evt)
 {
 case HCI_DISCONNECTION_COMPLETE_EVT_CODE:
 {
 break;
 }
 case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
 {
 break;
 }
 }
}

In both cases, I never go to this function even if I am connected to the device it sends data through notify.

4 months ago, when I was working with the stm32 sequencer for the Bluetooth, the first function was working and correctly broke when I connected the device to the phone (I checkout to the branch to check)

Environment :

  • Target: STM32wb55
  • Target OS: FreeRTOS
  • Host OS: Windows
  • Toolchain: stm32cubeIDE

Do you have an idea of what can cause the issue?
Thanks in advance

This topic has been closed for replies.

2 replies

Senior III
March 11, 2025

When a connection is established, your STM32 should store the connection handle. If not, it might be an issue with aci_gap_set_event_mask(). Check if 

 

aci_gap_set_event_mask(GAP_EVT_MASK_ALL);

 

is set correctly in your BLE initialization.

PierreLAuthor
Associate II
March 11, 2025

The function

aci_gap_set_event_mask

Does correctly exist but

GAP_EVT_MASK_ALL

do not exist. I try to put 0xFFFF, 0x0002, 0x0020 in MX_APPE_Init, but it goes directly to the error Handler in the function. Moreover, the function aci_gap_set_event_mask is never call