2023-07-16 2:07 PM - last edited on 2023-07-20 3:32 AM by KDJEM.1
Hi How to make external OctoSPI loader for STM32H723zgt6 with octospi and w25q256
Thanks.
Solved! Go to Solution.
2023-07-19 6:11 PM
I can't spend hours debugging / fixing your project.
Based on my existing Winbond implementation https://github.com/cturvey/stm32extldr/blob/main/h7_w25q256/CLIVEONE-W25Q256_STM32H72X-PB2-PG6-PF8-PF9-PF7-PF6.stldr
2023-07-19 11:37 PM
Thank you very much, it worked great and the program is complete. God bless you in life. It would be even better if you could add the .flm file in the future. I live in Iran and our country is embargoed and I don't have access to paypal , otherwise I would have paid you
2023-07-20 5:53 PM - edited 2023-07-21 10:21 AM
Ok, so this is a Keil FLM for the H7 OCTO, here its a H7A0/H7B0 platform, but might also work for the H72x too. If not, I'll need to refactor the project to build for the other H7 part. https://github.com/cturvey/stm32extldr/blob/main/h7_w25q256/W25Q256_STM32H7AX-CUSTOM17.FLM
2023-07-21 5:27 AM - edited 2023-07-21 8:34 AM
One built pulling H723 includes https://github.com/cturvey/stm32extldr/blob/main/h7_w25q256/W25Q256_STM32H72X-CUSTOM17.FLM