cancel
Showing results for 
Search instead for 
Did you mean: 

H723 FDCAN1 and FDCAN2

PGrif.2
Associate III

Hi there,

I am using two STM32H723ZGT communicating via FDCAN2 instance (FDCAN, no bit rate switch, 12500 bit/s). Both controller use the same FDCAN initialization code, but different filter IDs.

As shown below, the message is transfered on receiver CAN_Rx (upper trace) and acknowledged on sender CAN_Rx (lower trace), but neither the HAL_FDCAN_RxFifo0Callback() nor HAL_FDCAN_RxFifo1Callback() is triggered. When the receiver is shut down, the ackowledge disapears, so the message seems stuck in the the CAN peripherial.

FDCAN messageFDCAN message

CAN instance 1 (CAN2.0) is used for communication with other periperhial devices an works as expected.

What am I missing?

Thanks in advance!

 

CAN2 initialization FDCAN for both controller

 

/* USER CODE END FDCAN2_Init 1 */
  hfdcan2.Instance = FDCAN2;
  hfdcan2.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
  hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
  hfdcan2.Init.AutoRetransmission = DISABLE;
  hfdcan2.Init.TransmitPause = DISABLE;
  hfdcan2.Init.ProtocolException = ENABLE;
  hfdcan2.Init.NominalPrescaler = 32;
  hfdcan2.Init.NominalSyncJumpWidth = 5;
  hfdcan2.Init.NominalTimeSeg1 = 32;
  hfdcan2.Init.NominalTimeSeg2 = 7;
  hfdcan2.Init.DataPrescaler = 1;
  hfdcan2.Init.DataSyncJumpWidth = 16;
  hfdcan2.Init.DataTimeSeg1 = 20;
  hfdcan2.Init.DataTimeSeg2 = 16;
  hfdcan2.Init.MessageRAMOffset = 196;
  hfdcan2.Init.StdFiltersNbr = 1;
  hfdcan2.Init.ExtFiltersNbr = 1;
  hfdcan2.Init.RxFifo0ElmtsNbr = 16;
  hfdcan2.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_64;
  hfdcan2.Init.RxFifo1ElmtsNbr = 16;
  hfdcan2.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_64;
  hfdcan2.Init.RxBuffersNbr = 0;
  hfdcan2.Init.RxBufferSize = FDCAN_DATA_BYTES_64;
  hfdcan2.Init.TxEventsNbr = 0;
  hfdcan2.Init.TxBuffersNbr = 0;
  hfdcan2.Init.TxFifoQueueElmtsNbr = 16;
  hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
  hfdcan2.Init.TxElmtSize = FDCAN_DATA_BYTES_64;
  if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN FDCAN2_Init 2 */

 

CAN2 Filter configuration

 

uint8_t CAN_ConfigCAN02Filter(uint8_t own_address)
{
	//
	uint8_t result = 0;
	FDCAN_FilterTypeDef canFilterConfig = { 0 };
	uint8_t filterindex  = 0;

	//
	canFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO1;

	//
	canFilterConfig.IdType = FDCAN_EXTENDED_ID;

	//
	canFilterConfig.FilterType = FDCAN_FILTER_MASK;

	//
	canFilterConfig.FilterID1 = own_address;	// canIdentifier
	canFilterConfig.FilterID2 = 0;				// mask: 0 => accept all messages

	//
	canFilterConfig.RxBufferIndex = 0;			// set to 0 if using FIFO
	//	canFilterConfig.IsCalibrationMsg = 0;

	//
	canFilterConfig.FilterIndex = filterindex;

	// configure the FDCAN reception filter
	result += HAL_FDCAN_ConfigFilter(&hfdcan2, &canFilterConfig);

	//
	filterindex += 2;

	// enable Rx interrupts
	result += HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0);
	result += HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_RX_FIFO1_NEW_MESSAGE, 0);

	// enable Tx interrupts
	result += HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_TX_COMPLETE, FDCAN_TX_BUFFER0);
	result += HAL_FDCAN_ActivateNotification(&hfdcan2, FDCAN_IT_TX_FIFO_EMPTY, 0);

	// configure global filter to reject all non-matching frames
	HAL_FDCAN_ConfigGlobalFilter(&hfdcan2,
			FDCAN_REJECT,
			FDCAN_REJECT,
			FDCAN_REJECT_REMOTE,
			FDCAN_REJECT_REMOTE);

	//
	return result;
}

 

CAN1 initialization CAN2.0 

 

 /* USER CODE END FDCAN1_Init 1 */
  hfdcan1.Instance = FDCAN1;
  hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
  hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
  hfdcan1.Init.AutoRetransmission = DISABLE;
  hfdcan1.Init.TransmitPause = DISABLE;
  hfdcan1.Init.ProtocolException = ENABLE;
  hfdcan1.Init.NominalPrescaler = 40;
  hfdcan1.Init.NominalSyncJumpWidth = 5;
  hfdcan1.Init.NominalTimeSeg1 = 10;
  hfdcan1.Init.NominalTimeSeg2 = 9;
  hfdcan1.Init.DataPrescaler = 1;
  hfdcan1.Init.DataSyncJumpWidth = 16;
  hfdcan1.Init.DataTimeSeg1 = 20;
  hfdcan1.Init.DataTimeSeg2 = 16;
  hfdcan1.Init.MessageRAMOffset = 0;
  hfdcan1.Init.StdFiltersNbr = 1;
  hfdcan1.Init.ExtFiltersNbr = 1;
  hfdcan1.Init.RxFifo0ElmtsNbr = 16;
  hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.RxFifo1ElmtsNbr = 0;
  hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.RxBuffersNbr = 0;
  hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.TxEventsNbr = 0;
  hfdcan1.Init.TxBuffersNbr = 0;
  hfdcan1.Init.TxFifoQueueElmtsNbr = 32;
  hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
  hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
  if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN FDCAN1_Init 2 */

 

 

 

 

23 REPLIES 23

I've seen it used in almost all application where multiple uC are present on the same board. also automotive grade applications... Where is not recommended?

 

I've seen it used in almost all application where multiple uC are present on the same board. 


Intriguing. What kind of commercial products have these applications? 

 

 


also automotive grade applications...

What automotive manufacturer and node application have you seen this on? BCM, ECM? IPC, DDM?

What bus type? GMLAN/SWCAN? MSCAN? HSCAN? I'd like to investigate. 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Again: as ST we don’t recommend that config and we don’t guarantee the behavior. If you want to implement it in your application you do it on your own responsability. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Some device need to have multiple mcu on the same board (e.g. for redundancy). Quite often (at least on my experience) use or SPI commuincation or CAN communication.

Application like on board battery charger, motor drivers, ECU but also in railway application etc

When CAN communication is used I've never seen used transceiver in this case and for internal CAN commuincations a custom CAN protocol is used .