2024-02-12 04:05 PM
Hello, i'm testing FDCAN in my stm32g431 and it doesn't work well. Messeges goes throught it, even if ID doesn't match (TxHeader.Identifier = 0x102 shouldn't pass, but it does!)
static void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;
hfdcan1.Init.AutoRetransmission = DISABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = DISABLE;
hfdcan1.Init.NominalPrescaler = 3;
hfdcan1.Init.NominalSyncJumpWidth = 1;
hfdcan1.Init.NominalTimeSeg1 = 2;
hfdcan1.Init.NominalTimeSeg2 = 2;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 1;
hfdcan1.Init.DataTimeSeg1 = 1;
hfdcan1.Init.DataTimeSeg2 = 1;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 1;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0; // Use the first filter bank
sFilterConfig.FilterType = FDCAN_FILTER_MASK; // Specify the filter type
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0; // Store matching messages in RX FIFO 0
sFilterConfig.FilterID1 = 0x103; // filter
sFilterConfig.FilterID2 = 0x103; // mask
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK) {
// Handle error
}
}
Solved! Go to Solution.
2024-02-21 01:07 AM
Hello,
You need to configure the global filter. For example:
HAL_FDCAN_ConfigGlobalFilter(&hfdcan1,
FDCAN_REJECT,
FDCAN_REJECT,
FDCAN_REJECT_REMOTE,
FDCAN_REJECT_REMOTE);
2024-02-13 05:14 AM
configurating global filter was a solution C:
2024-02-21 01:07 AM
Hello,
You need to configure the global filter. For example:
HAL_FDCAN_ConfigGlobalFilter(&hfdcan1,
FDCAN_REJECT,
FDCAN_REJECT,
FDCAN_REJECT_REMOTE,
FDCAN_REJECT_REMOTE);