2024-05-29 11:47 PM
Hi there!
I 've got a project where i use the STM32H757 dual core (Riverdi 7")
the M7 core
the M4 core
When starting the M7 core first and then the M4 core for debugging (AN5361 - STLink GDB Server) the Ethernet connection is interrupted (no successfull ping), when the M4 debug session starts.
M4 DMA is set behind the user_heap_stack in the .ld file
.dma_buffer :
{
. = ALIGN(8);
*(.dma_buffer)
} >RAM
Cheers!
2024-05-31 09:19 AM
Hello @PGrif.2 ,
Is this behavior only visible in Debug Mode only? can please also specify the tools version you are using as well as the Ethernet Driver version if you started the project using CubeMX it will help to see the way you configured FreeRtos and the assignment of the LWIP stack as well. Also if you can send a project to help us reproduce this behavior it would be great .
Regards
2024-06-03 11:26 PM - edited 2024-06-04 12:03 AM
Hi @STea !
The behaviour is also visible in normal start up without a debug probe using just Power over Ethernet.
HW was purchased in April/May 2024
the tool chain contains of
there are reported (but not solved) issues with the generation of the MX_XXXX_Init() section by CubeMX 6.11.1
Re: H7 Riverdi screen adding DMA to M4 core leads ... - STMicroelectronics Community
I will not use the latest FW_H7 V1.11.2 since there are reported issues with the LWIP section
Re: CubeMX 6.11.1 removes LWIP part of H7 .ioc fil... - STMicroelectronics Community
Can't enable LWIP on STM32H745 Cortex-M7 only - STMicroelectronics Community
I used Adam Berlingers post How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community (Thank you Adam!) but changed the MPU and ETH values as shown below, since the orginal posted values lead to the same issues as described here.
M7 settings for Ehternet
M4 settings for ADC to DMA
ETH connection
for more details see the attads .ioc and load files.
Thanks for your help
Cheers!
2024-06-03 11:42 PM - edited 2024-06-03 11:48 PM
CubeMX 6.11.1 fun fact
The project is taken form the provided TouchGFX Riverdi example and can be build and simulated successfully in TouchGFX Designer, but when opening the .ioc file in CubeMX 6.11.1 it shows no selected TouchGFX ...
... even when it is in the .ioc file, as shown below on left side. When reselecting and saving in CubeMX it will disapear from .ioc file as shown below on the right side.
2024-06-05 08:52 AM
Hello @PGrif.2 ,
I don't seem to get the way you are setting your regions and sizes in MPU config, and it seem to be you issue. you need to make sure of the size of your regions and have in mind the Memory aliasing happening between CM4 and CM7 to get this right.
to make sure you are getting the MPU config right check this helpful youtube tutorial.
regarding the issue with LWIP configuration it will be fixed in the next release.
2024-06-13 08:19 AM
Hello @PGrif.2 ,
any updates on this issue?