cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32F413 use the LSE generation 1 or 2?

Stefan W
Associate II

The document AN2867 (Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs) defines to groups for the F4 series: F4_g1 and F4_g2. There is a list with the controllers for each group, but the STM32F413 is not mentioned.

4 REPLIES 4
TDK
Guru

That's referring to the ability to change the LSE drive strength. The STM32F413 has an LSEMOD bit in the RCC_BDCR register, so it would be in group 2.

If you feel a post has answered your question, please click "Accept as Solution".
Imen GH
ST Employee

Hello,

I confirm that the LSE generation of STM32F413 is not mentioned and it will be added in next release. This LSE has two drive level and it is generation 2.

Regards 

FWagn.1
Associate

Where is the List?

Best Regards

In AN2867:0693W00000HnXGIQA3.pngAlso in footnote to Table 7.

JW