cancel
Showing results for 
Search instead for 
Did you mean: 

IAR project generated by TouchGFX Designer cannot be compiled

rhine1012
Associate II

1.  Hardware is STM32U5A9J-DK.

2. Using TouchGFX Designer-Demo6 to 'Generate Code', 'Run Simulator', 'Program and Run Target', STM32U5A9J-DK works well.

3. When I want to compile the generated code in step 2 by IAR IDE, error occurs:

'F:/3_softprj/02_stm32cube/touchgfx/gfx0207/Middlewares/ST/touchgfx_components/gpu2d/NemaGFX/lib/core/cortex_m33/IAR8.x/nemagfx_core_release.a', needed by 'F:/3_softprj/02_stm32cube/touchgfx/gfx0207/EWARM/STM32U5A9J-DK-FreeRTOS/Exe/STM32U5A9J-DK-FreeRTOS.out', missing and no known rule to make it

rhine1012_0-1738925782587.png

There is no IAR8.x in directry 'F:/3_softprj/02_stm32cube/touchgfx/gfx0207/Middlewares/ST/touchgfx_components/gpu2d/NemaGFX/lib/core/cortex_m33', besides gcc.

rhine1012_1-1738925948083.png

IAR version is 9.32.

why does the compiling error occur?

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
LouisB
ST Employee

Hello @rhine1012 ,


Please refer to the documentation here : 1. Create Project | TouchGFX Documentation,

 

BR,

Louis BOUDO
ST Software Engineer | TouchGFX

View solution in original post

1 REPLY 1
LouisB
ST Employee

Hello @rhine1012 ,


Please refer to the documentation here : 1. Create Project | TouchGFX Documentation,

 

BR,

Louis BOUDO
ST Software Engineer | TouchGFX