‎2024-07-08 11:23 PM
I found the motor value using the Motor Profiler 5.4.8 program (P-NUCLEO-IHM002).
(Figure1)
The Motor Pilot_6.3.0 program does not connect using UART.(Discover Board / Launch Profiler)
(Figure3)
Even if I change the UART Speed, the "Port Open and try to configure the board" error only appears.
(Figure4)
I bought EVSPIN32G4 to run the motor at 60v voltage level.
However, I understand that motor measurement is currently not possible with the Motor Profiler 5.4.8 program.
In that case, you need to measure it in the Motor Pilot_6.3.0 program.
I can't check anything because the connection isn't working.
MC_Workbench cannot create a project because there is no motor with similar specifications.
Since I cannot receive the motor value from the motor manufacturer, I have to proceed through measurement. Please tell me how I can do this.
‎2024-07-09 7:50 AM
Hello @SUNGHWANCHO,
Please have a look to How_To_manually_configure_the_motor_parameters link.
‎2024-07-09 5:55 PM
After purchasing EVSPIN32G4, I only updated ST-LINK after connecting Micro USB.
It is connected to the motor as shown below.
The board cannot be connected in ST Motor Pilot.
 
How do I connect?
‎2024-07-09 6:44 PM
MCSDK 6.3 Profile need user to add FW manually by create new project ,you may refer to MCSDK document in "about" ICON and search "Motor Profiler Application Note"