cancel
Showing results for 
Search instead for 
Did you mean: 

LwIP heap memory in DTCMRAM

iTTy
Associate III

Hi there!

I already configured LwIP package and make it work on a NUCLEO-H755ZIQ following @Adam BERLINGER gude in the Knowledge base section:

https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308 

Well, trying to move the LwIP heap memory to a larger memory location I experienced a n unexpected issue:

When I locate the heap in the DTCMRAM of the M7 core, communication will no more work at all(no ping, no tcp connection...).

Locating it in D1 (AXI RAM) or D3 RAM all work as expected.

I checked also the MPU configurations ad all seems correct, it seems that in DTCMRAM there is a different behavior.

 

Just for my comprehension, there is something wrong in locating such heap into the DTCMRAM?

Thanks in advance! 

iTTy

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

I'm not an ETH expert but seems the heap is used by one of DMA1/DMA2 masters that does not have access to DTCM  RAM.

From RM0399 reference manual:

SofLit_0-1712829693355.png

Same as: https://community.st.com/t5/stm32cubeide-mcus/adc-with-dma-in-scan-mode-is-not-resulting-in-call-to-hal-adc/m-p/660253

EDIT: I forgot to mention the ETH master which also doesn’t have access to the DTCM.

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

I'm not an ETH expert but seems the heap is used by one of DMA1/DMA2 masters that does not have access to DTCM  RAM.

From RM0399 reference manual:

SofLit_0-1712829693355.png

Same as: https://community.st.com/t5/stm32cubeide-mcus/adc-with-dma-in-scan-mode-is-not-resulting-in-call-to-hal-adc/m-p/660253

EDIT: I forgot to mention the ETH master which also doesn’t have access to the DTCM.

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Intresting!

Just a clarification: in my application project I don't settled up any DMA usage for the ethernet commnunication.

Could be that LwIP package is using DMA in a "hidden" way?

Several masters such as DMA1, DMA2, ETH (used in your case) etc .. don't have access to DTCM RAM. Look at the table 2 in the RM0399 I've already shared.

I've already edited my previous post.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
LCE
Principal

I confirm SofLit's post, the ETH DMA (neither any other DMA :( ) cannot access DTCM.
I had to place it in D1 AXI SRAM (H7xx).