cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE generate Too Big BIN file for STM32WL

Karthi
Associate II

Hi

We re trying to compile LoRaWAN_END_Node project from STM32WL Cube library. CubeIDE generate 402 MB  bin File. Can someone from STteam  look into this.


MCU STM32WLE5CC
Mac Verion 1.0.3
WL 1.3.1

Karthi_0-1743008981009.png

 

Karthi_0-1743009314808.png

 

 

Karthi_1-1743009341876.png

Karthi_2-1743009366258.png

 

Karthi_0-1743009497249.png

 

 

 

 

ld file

 

/*
******************************************************************************
**
**  File        : LinkerScript.ld
**
**  Author      : STM32CubeIDE
**
**  Abstract    : Linker script for STM32WL55xC Device
**                      256Kbytes FLASH
**                      64Kbytes RAM
**
**                Set heap size, stack size and stack location according
**                to application requirements.
**
**                Set memory bank area and size if external memory is used.
**
**  Target      : STMicroelectronics STM32
**
**  Distribution: The file is distributed as is without any warranty
**                of any kind.
**
**  Note        : For specific memory allocation, linker and startup files must be customized.
**                Refer to STM32CubeIDE user guide (UM2609), chapter "Modify the linker script".
**
*****************************************************************************
** @attention
**
** Copyright (c) 2021 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
*****************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(RAM1) + LENGTH(RAM1); /* end of "RAM1" Ram type memory */

_Min_Heap_Size = 0x200; /* required amount of heap  */
_Min_Stack_Size = 0x800; /* required amount of stack */

/* Memories definition */
MEMORY
{
  RAM1   (xrw)   : ORIGIN = 0x20000000, LENGTH = 32K
  NVM_RAM (rw)   : ORIGIN = 0x20008000, LENGTH = 4K
  RAM2   (xrw)   : ORIGIN = 0x20009000, LENGTH = 28K
  FLASH   (rx)   : ORIGIN = 0x08000000, LENGTH = 248K
  USER_Key_region_ROM (rx)    : ORIGIN = 0x0803E500, LENGTH = 768
}

/* Sections */
SECTIONS
{
  /* The startup code into "FLASH" Rom type memory */
  .isr_vector :
  {
    . = ALIGN(8);
    KEEP(*(.isr_vector)) /* Startup code */
    . = ALIGN(8);
  } >FLASH

  /* The program code and other data into "FLASH" Rom type memory */
  .text :
  {
    . = ALIGN(8);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)

    KEEP (*(.init))
    KEEP (*(.fini))

    . = ALIGN(8);
    _etext = .;        /* define a global symbols at end of code */
  } >FLASH

  /* Constant data into "FLASH" Rom type memory */
  .rodata :
  {
    . = ALIGN(8);
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    . = ALIGN(8);
  } >FLASH

  .ARM.extab   : {
    . = ALIGN(8);
    *(.ARM.extab* .gnu.linkonce.armextab.*)
    . = ALIGN(8);
  } >FLASH

  .ARM : {
    . = ALIGN(8);
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
    . = ALIGN(8);
  } >FLASH

  .preinit_array     :
  {
    . = ALIGN(8);
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array*))
    PROVIDE_HIDDEN (__preinit_array_end = .);
    . = ALIGN(8);
  } >FLASH

  .init_array :
  {
    . = ALIGN(8);
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array*))
    PROVIDE_HIDDEN (__init_array_end = .);
    . = ALIGN(8);
  } >FLASH

  .fini_array :
  {
    . = ALIGN(8);
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array*))
    PROVIDE_HIDDEN (__fini_array_end = .);
    . = ALIGN(8);
  } >FLASH

  .USER_embedded_Keys : {
    . = ALIGN(8);
    *(.USER_embedded_Keys)
    . = ALIGN(8);
  } >USER_Key_region_ROM

  /* Used by the startup to initialize data */
  _sidata = LOADADDR(.data);

  /* Initialized data sections into "RAM1" Ram type memory */
  .data :
  {
    . = ALIGN(8);
    _sdata = .;        /* create a global symbol at data start */
    *(.data)           /* .data sections */
    *(.data*)          /* .data* sections */
    *(.RamFunc)        /* .RamFunc sections */
    *(.RamFunc*)       /* .RamFunc* sections */

    . = ALIGN(8);
    _edata = .;        /* define a global symbol at data end */

  } >RAM1 AT> FLASH

  /* NVM RAM Data */
  LW_NVM_RAM (NOLOAD) :
  {
    . = ALIGN(8);
    *(.bss.LW_NVM_RAM)
    *(.bss.LW_NVM_BACKUP_RAM)
    . = ALIGN(8);
  } >NVM_RAM

  /* Uninitialized data section into "RAM1" Ram type memory */
  . = ALIGN(8);
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section */
    _sbss = .;         /* define a global symbol at bss start */
    __bss_start__ = _sbss;
    *(.bss)
    *(.bss*)
    *(COMMON)

    . = ALIGN(8);
    _ebss = .;         /* define a global symbol at bss end */
    __bss_end__ = _ebss;
  } >RAM1

  /* Data section into "RAM1" Ram type memory: Non-backup RAM1 dedicated to CM4 */
  . = ALIGN(8);
  RAM1_region :
  {
    _sRAM1_region = .;         /* define a global symbol at section start */
    *(.RAM1_region)

    . = ALIGN(8);
    _eRAM1_region = .;         /* define a global symbol at section end */
  } >RAM1

  /* Data section into "RAM2" Ram type memory: Backup RAM2 dedicated to CM4 */
  . = ALIGN(8);
  RAM2_region :
  {
    _sRAM2_region = .;         /* define a global symbol at section start */
    *(.RAM2_region)

    . = ALIGN(8);
    _eRAM2_region = .;         /* define a global symbol at section end */
  } >RAM2

  /* User_heap_stack section, used to check that there is enough "RAM1" Ram  type memory left */
  ._user_heap_stack :
  {
    . = ALIGN(8);
    PROVIDE ( end = . );
    PROVIDE ( _end = . );
    . = . + _Min_Heap_Size;
    . = . + _Min_Stack_Size;
    . = ALIGN(8);
  } >RAM1

  /* Remove information from the compiler libraries */
  /DISCARD/ :
  {
    libc.a ( * )
    libm.a ( * )
    libgcc.a ( * )
  }

  .ARM.attributes 0 : { *(.ARM.attributes) }
}

 

 

1 REPLY 1
Pavel A.
Super User

This is because the executable contains several data blocks at addresses very far away: 08000000 and 20008000.

The tool must output a single flat binary so it just does its best and fills the huge hole(s). Bottom line: the plain .bin file is not optimal format for this program. Why not just use the .hex?