2024-05-04 05:52 AM
In the X-Cube Display Package there is a HelloWorld Application for X-NUCLEO-GFX02Z1 with a NUCLEO-H723ZG. Is it possible to change it in a way to make it on Nucleo-H755ZI-Q running?
Otherwise, is there a step by step manual to get the display X-NUCLEO-GFX02Z1 on a Nucleo-H755ZI-Q running?
Or is there an already exisiting project to download?
Since I programmed everything with the Nucleo-H755ZI-Q I would like to stay on this system. Is there another display to get fast running on a Nucleo-H755ZI-Q?
2024-05-04 04:46 PM
Hello @guc and welcome to the Community 🙂
You can use a ready-to-use example and make it work on Nucleo-H755ZI-Q.
You can also start and create your own project on NUCLEO-H755ZI-Q using STM32CubeMX and integrate the X-CUBE software package.
I advise you to follow these resources which provide a step-by-step on how to get started and configure a project in STM32CubeMX:
2024-05-05 12:53 PM
Hello Imen.D
I downloaded X-CUBE-DISPLAY.3.0.0 and found a Helloworld project for NUCLEO-H723ZG. I tried to make it working with NUCLO-H755ZI-Q. But at the very end there were so many thing which were not fitting so I needed to give up. One example is OSPI. Apperantly supported by H723ZG but not with H755ZI-Q.
How should I make it work from your point of view?
The UM2787" and the "1. Create Project | TouchGFX Documentation" I already worked through. But there is a problem with H755ZI-Q with the X-CUBE-DISPLAY.3.0.0 package. Somehow it does not work properly even I'm using Cube IDE 12.1. Taking as a component (SW Packs-->Select Components) GFX02Z1 does not work at all. Taking ILI9341 does also not look like it is described in the manual (see screenshot). I also added the CUBE IDE Project as attachment.
And TouchGFX also does not support the combination NUCLO-H755ZI-Q with GFX02Z1.
So how shall i proceed here?
I'm a little bit disappointed also because it is written that GFX02Z1 is compatible with NUCLO-H755ZI-Q.
Anyway thanks for your support!
2024-05-06 05:50 AM
Hi @guc ,
There is a short description of how to install TouchGFX X-CUBE-TOUCHGFX 4.23.2 is out! - STMicroelectronics Community:
"Attention: If X-CUBE-TOUCHGFX 4.23.2 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-2.zip file to install the new pack inside STM32CubeMX."
You can follow this section Installation | TouchGFX Documentation and show how to install TouchGFX as well as all the necessary components in the toolchain required.
2024-05-06 07:02 AM
Hi @Imen.D
TouchGFX is not the purpose I actually have. Main purpose I have is to use the display without any user interaction.
So the bigger points I have a re the following:
"I downloaded X-CUBE-DISPLAY.3.0.0 and found a Helloworld project for NUCLEO-H723ZG. I tried to make it working with NUCLO-H755ZI-Q. But at the very end there were so many thing which were not fitting so I needed to give up. One example is OSPI. Apperantly supported by H723ZG but not with H755ZI-Q.
How should I make it work from your point of view?
The UM2787" and the "1. Create Project | TouchGFX Documentation" I already worked through. But there is a problem with H755ZI-Q with the X-CUBE-DISPLAY.3.0.0 package. Somehow it does not work properly even I'm using Cube IDE 12.1. Taking as a component (SW Packs-->Select Components) GFX02Z1 does not work at all. Taking ILI9341 does also not look like it is described in the manual (see screenshot). I also added the CUBE IDE Project as attachment."
Thank you and regards Guc