ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Clarify ST25RU3993 Availability

In an earlier post, the ST25RU3993 was EOL with no replacement.https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/replacement-for-st25ru3993-coming/m-p/60581 Now the ST25RU3993 is again available and active. Is there an official period this p...

Jeff C by Associate II
  • 1225 Views
  • 4 replies
  • 0 kudos

Resolved! ST25R3916B RF power output

Hi, it's not clear the deliverable power of the ST25R3916B. it seems 1.6W in balance output configuration. On the datasheet is written only that there is a dynamic power output, on the first page then no more other information, and there are no regis...

Resolved! ST25DV64K ignoring address in GPO interrupt request

I opened a ticket in the ST online support system and was pointed to this forum for support.I have a device that uses the ST25DV64K and I'm talking to it using the ST25R3911B-DISCO board and the corresponding Discovery GUI from ST. The documentation ...

nhedler by Associate
  • 840 Views
  • 1 replies
  • 0 kudos

Resolved! ST25R3911B DISCO

Hi,I currently have a LabVIEW 32 bit application that uses the ST M24LR-DISCOVERY evaluation kit via the CR95HF.dll, and now have a need to update this application to use the ST ST25R3911B DISCO DISCOVERY kit via the ST25R3911DISCOComm.dllIs there an...

John63 by Associate
  • 1553 Views
  • 3 replies
  • 0 kudos

Resolved! BLE-OOB pairing on iOS using the ST25DV64KC-DISCO

I have already purchased the ST25DV64KC-DISCO board.I want to perform Bluetooth® Low Energy OOB validation.The user manual (UM2949) states that "ST BlueNRG module" is required.Specifically, which product should I purchase and connect?Please let me kn...

tm7177 by Associate
  • 2194 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with ST25R95 and ISO15693

Hello, I have a similar problem as it was asked herehttps://community.st.com/t5/st25-nfc-rfid-tags-and-readers/rfal-demo-question/m-p/157070#M2943 I am trying to read 15693 tags with a board I designed myself.I adjusted the RFAL library to use my own...

Resolved! NFC ndef format

Hi,I have a use case where I need to read and write to an NFC tag. The read and write operation will always be done by an MCU (via st25R) and not by any other device (eg:- android device).Should I use the NDEF format for the data in this case ? What ...

Luke_abc by Associate III
  • 3966 Views
  • 3 replies
  • 2 kudos

Resolved! Problem with st25dv16k ISO 15693 iOS communication

Hello!I am trying to read some blocks from a iso 15693 tag. I can do it with Android without any problem. But when I try to do it with iOS I always receive the response [255,255]. What does it mean?For example:22 33 E0 02 51 00 02 4E BE 55 08 00 32 0...

koy by Associate II
  • 1552 Views
  • 4 replies
  • 0 kudos