2023-10-12 6:19 AM
I am attempting to use the ST25R3911B-DISCO plugged into Android and I am wondering if this is possible. Right now, I am using the ST25AndroidDemoApp with Android Studio and I am able to use NFC from my android tablet and find a ST25 tag. My end goal is instead of using the NFC of my android tablet, I want to try and use the NFC from the ST25R3911B-DISCO which would be connected to the android tablet through USB. Is this possible, and if so, how might I go about implementing this?
Solved! Go to Solution.
2023-10-12 9:17 AM
Hi,
I don't know the ST25SDK in detail but I think yes, this is what is used for Windows PC. Similar will be needed for Linux but I guess some parts of it may even be re-used.
BR, Ulysses
2023-10-12 6:56 AM
Hello itsgimbi,
I think what you describe nobody has done before and I also expect huge efforts which I expect will not pay off for you. Giving some hints for you:
Those two don't really fit together and for integration one would need to become experts on NCI, ST25R3911B-DISCO protocol and on NFC.
Best Regards, Ulysses
2023-10-12 7:08 AM
Hello Ulysses,
Thanks for the quick reply. To follow up, there is a ST25 Java SDK introduction presentation that I found online that says on Android that "The RF reader interface implementation is directly plugged on Android SDK APIs (thin wrapper)." Does this mean that it is possible to plug the ST25R3911B-DISCO into my Android tablet and pull up a GUI to see if there is communication between the board and a ST25 tag? Or is it just in general not possible to run the ST25R3911B-DISCO on Android? Here is the link to the presentation if you unaware of it. ST25SDK presentation
2023-10-12 7:36 AM
Hi,
Your question sounded like you wanted to replace the stock Android NFC with ST25R3911B-DISCO. I.e. replace "Android RF reader" with ST25R3911B-DISCO. Any app/system using NFC would then implicitly use ST25R3911B-DISCO. That is what I was answering below.
What you describe now would be to use ST25SDK from one Android app to use the ST25R3911B-DISCO. This would be a bit easier, however you still need to hack into the Android system to be able to use JNI/control the USB HID to execute the proprietary USB HID protocol spoken by ST25R3911B-DISCO.
On Windows PC a DLL is provided which is used by some Reader implementation to drive the board. This you would need to replicate somehow on Android.
BR, Ulysses
2023-10-12 7:50 AM
Hi,
So just to sum it up, if I am trying to make an app to use the ST25R3911B-DISCO NFC which would be connected to an android tablet through USB instead of the tablet's NFC, I would try to use JNI and control the USB HID.
2023-10-12 7:59 AM - edited 2023-10-12 7:59 AM
Hi,
yes, JNI or whatever other means you have to directly control the USB HID device (don't have experience on Android/Linux here).
Regards, Ulrich
2023-10-12 8:15 AM
Hi,
Thanks for the clarification. In the ST25SDK download, there a ST folder that contains support files for reader discovery kits based on CR95HF, ST25R3911B and ST25R3916 that includes RFReaderInterface implementation and JNI and dynamic library dependencies according to the readme. Could this be of help for me or are they used for something else?
2023-10-12 9:17 AM
Hi,
I don't know the ST25SDK in detail but I think yes, this is what is used for Windows PC. Similar will be needed for Linux but I guess some parts of it may even be re-used.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.