ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Impedance matching and RFO level definition

Hello,i want to design a new antenna layout with the ST253911b chip.It is recommended to match the antenna across RFO1 and RFO2 to a load impedance of 10 Ohm.Do i have to change the register "RFO normal level definition register" adress 27h to 10Ohm?...

PeterSPX by Associate II
  • 1086 Views
  • 3 replies
  • 0 kudos

Resolved! ST25DV Communication error when reading I2C

Hello allI use ST25DV64K.If the I2C communication is normal, it returns ACK after receiving data, and after receiving the last data, it returns NACK response and issues Stop Condition.If the I2C communication is abnormal, and the master issues a stop...

MMoro.4 by Associate II
  • 1792 Views
  • 2 replies
  • 0 kudos

Resolved! ST25RU3993-HPEV sensitivity

Hi,We tested the receiving sensitivity of the RFID reader evaluation kit ST25RU3993-HPEV, and the actual measurement is -66dBm, but the sensitivity given in each document is -77dBm.The sensitivity given here(-77dBm) is the sensitivity of the ST25RU39...

Fma.1 by Associate II
  • 2425 Views
  • 12 replies
  • 0 kudos

Resolved! How can we read/write using SPI

Hi,I don't really understand the datasheet of the ST25R3916 IC chip.At page 53, they show an exemple of a direct write command. As I understand, we need to send 1-1-C5-C4-C3-C2-C1-C0. When I check table 13 to see the command code that go for bits C5....

ANaud.1 by Associate II
  • 5741 Views
  • 20 replies
  • 0 kudos