I use passive RFID tag with NFC03A1 card reader, I have create a little program to detect RFID tag, the range is up to 5 centimeters. Is there a way or a configuration to increase this range ?Thank you in advance.
I have planned to use sticker tags (can be ISO1443 or 15693). If i decide to use X-NUCLEO-NFC06A1 with ISO15693 sticker tags, what would be the detection range ? Thank you in advance.