ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Tips for triggering i_lim? (NFC WLC)

Hello,I've changed the impedance matching network on the NFC06A1 such that the system is resonant at 13.56MHz with an impedance of 2.6 ohms. The reader is in 5V mode with the regulator display register measuring 4.3V at VDD_RF. I have set the output ...

OSilv.1 by Associate II
  • 2265 Views
  • 10 replies
  • 0 kudos

Resolved! How to gen2ReadFromTag with ST25ru3993 ?

Hi ST,We are trying to integrate a ST25ru3993 with a new µC. We managed to detect and list tags using inventoryGen2() command, but we are struggling with the gen2ReadFromTag() one:In the doxygen embedded in gen2.h code, we can see the following examp...

TCrav.1 by Associate III
  • 644 Views
  • 1 replies
  • 0 kudos

Resolved! Questions on ST25RU3993-HPEV output power

Hello ST,We are working with the ST25RU3993-HPEV board to evaluate the RFID chip.We have performed measurement of the output level on the antenna port and below are the obtained results:For the internal PA:Output level set using ST GUI / Expected out...

SPhun.1 by Associate II
  • 800 Views
  • 2 replies
  • 0 kudos

Resolved! Enter a password on the NFC Tap iOS app

How do I enter a password on the NFC Tap iOS app when the keyboard covers the action buttons?I'm trying to password protect a ST25TA02KB using NFT Tap for iOS, and having some difficulty. First, it's giving me a, "This is not a type 4A tag" error. If...

JVern.4 by Associate
  • 1600 Views
  • 3 replies
  • 0 kudos

Resolved! Out of Band Pairing

Hi,I have a project where we use the STM32WB55 with the ST25R3911B as NFC module for OOB pairing.I couldn't find any example for OOB pairing flow.My start point is the p2p_server example and I can see there are:BleApplicationContext.BleApplicationCon...

~Amit~ by Associate III
  • 4564 Views
  • 14 replies
  • 0 kudos

Resolved! How to use DLL CR95HF.dll on VB.NET?

Hi eveyone,I need to use the CR95HF.dll library on a VB.NET application but when i try insert on the project i get an error.I think this library is VB compatible only but i dont sure about this.Maybe anyone know how to port this library to be used on...

Dosan by Associate III
  • 3753 Views
  • 14 replies
  • 0 kudos