ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to configure GPO pin on ST25DV

Hi,I'm trying to set the GPO static register to 0xF1 to get corresponding interrupts.I am presenting the password first and then configuring GPO register at address 0000.Here is the program-NFCTAG_StatusTypeDef Set_GPO_reg(uint16_t flags) // Here fl...

Shruthi by Associate II
  • 972 Views
  • 3 replies
  • 0 kudos

Resolved! NFC Tap iOS app vs. NFC Tap Android app and FTM

We are developing both an Android and iOS app that leverages FTM from the ST25DV chip. In the Android version of the NFC Tap app, we can send custom commands and interact with FTM. However, in the iOS app, there is no "send custom command" screen. I ...

Mariano1 by Associate II
  • 940 Views
  • 3 replies
  • 0 kudos

Resolved! NFC Tap iOS app does not build.

I have downloaded the source of the iOS NFC-Tap app (version: en.STSW-ST25IOS002_v3.8.0). When I build the project in xCode, I receive the following error:en.STSW-ST25IOS002_v3.8.0/NFCTap/SwiftTryCatch/SwiftTryCatch.h:30:11: 'STException.h' file not ...

Mariano1 by Associate II
  • 838 Views
  • 3 replies
  • 0 kudos

Resolved! What's happening with the CR95HF RX resistance?

If you look into the AN4327 CR95HF transceiver antenna tuning circuit with EMI filter you see:I assume this means 22 pF capacity in parallel with 80 kOhm resistance. But when you open the recommended Excel sheet you see:Until this moment this was sup...

0693W00000JP3eyQAD.png 0693W00000JP3fhQAD.png 0693W00000JP3guQAD.png
RDien by Associate III
  • 563 Views
  • 2 replies
  • 0 kudos

Resolved! Apple VAS compatibility

Hello,I have been requested to have our RFID reader compatible with Android, iOS and physical cards.Android can perform HCE and NDEF messages can be read with our current reader (ST25R95). So far, so good.But, it seems apple is forcing to use Apple V...

Jhern.1 by Associate II
  • 2548 Views
  • 1 replies
  • 0 kudos

Resolved! Reading emulated cards with St25r95 / St95hf

Hello,I am trying to read data from iOS/Andriod App with my reader.Currently, my reader is based on st25r95 and it is in tag detector mode waiting for physical cards. Everthing is ok so far. Now I need to wakeup and get data from smartphone or pshysi...

Jhern.1 by Associate II
  • 1890 Views
  • 6 replies
  • 0 kudos