Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

smd marking

HELLO. CAN SOMEONE HELP ME IDENTIFY THIS CIRCUIT WHICH HAS THE NOTATION OF L4T . IT APPEARS TO BE A MOSFET BUT I'M NOT SURE BECAUSE I CAN'T FIND ANY REFERENCE ABOUT IT ANYWHERE. BECAUSE IT HAS 8 PINS. ITS DIMENSIONS ARE 2 X 2 X 1 MM. THANK YOU FOR AN...

STM8 Manual Clock Switching Bug

Hi,I guess there is a bug in manual clock switching (file: stm8s_clk.c function:CLK_ClockSwitchConfig:( /* Wait until the target clock source is ready */ while((((CLK->SWCR & CLK_SWCR_SWIF) != 0 ) && (DownCounter != 0))) { DownCounter--; }Mus...

STC4054GR

Good morningI must work to a board not projected from me with STC4054GR.The desgner has connect a led between VCC and pin CHRG (with a resistor) like a feedback for see the status (charging or not)I'm working with 2 board and i see 2 different behavi...

Resolved! STM32CubeMX MATLAB Hardware Setup

Hello team!! Perhaps this issue is solved somewhere, just want to be pointed on the right direction.Recently I got two NUCLEO boards (G474 & F334) and wnated to make a fast prototype on them, the first thing I did is the simple "blinky" prog to check...