TS514IN
Is this part Non-Rohs? Date Code 0234. I see the newer part TS514AID look to be Rohs. Where can we look up part's to see if they are Rohs or Non-Rohs?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Is this part Non-Rohs? Date Code 0234. I see the newer part TS514AID look to be Rohs. Where can we look up part's to see if they are Rohs or Non-Rohs?
Hi,I have an STM8S103F3P6 based development board & I wanted to know if it would be possible to execute program code from an external flash memory?Regards,Aditya.
Hi,I'm using L9678P. I’d like to confirm the specific definitions of these parameters:Is 1~10KΩ the detectable range?Are the conditions in the "Condition" column strongly correlated with the parameter values?What does "Equivalent to resistance range"...
Hello,I want to connect STM8S003 & ADXL345 (accelerometer) using SPI 3wire mode (lines ~CS, SCK & MOSI as single bidirectional data line).According to 'RM0016 Reference manual STM8S...', the register SPI_CR2 of STM8S has BDM (Bidirectional data mode ...
Hi, all. I've been beating my head against this problem for a few days now. I'm not getting any output from an STW81200 frequency synthesizer. I used the schematic from the eval board except that the reference is a crystal oscillator. Power is suppli...
Hello, this is the ECMF4-40A100N10(MIPI DSI ESD protection). I want to implement it in my design and I was wondering if it matters to connect your positive differential pair signals to D1+ and D2+ and negative to D-. Or can acually flip them? So I c...
Hi, I'm using STM32H745ZI for 4G LTE Communication Quectel EC200U-CN to transmit message using UART in Asynchronous mode, if I send continuous message then I'm getting this ................ ATAT+CPIN?AT+CMGF=1AT+CMGD=1,4AT+CSCS="GSM"AT+CSCA="91984908...
HI ST teams, I 've purchased STPM4RasPIV21 to test our SPI master device. I'v observed this TPM IC uses wait state when communication. Please help share behavior model(verilog) for SPI master simulation. Thanks a lot.
I've set up two different STUSB4500 ICs, my first board, when plugged in will fluctuate its output (measured from the output of the MOSFET) from 0 to 5V every few seconds or so. EDIT: I went probing on this first board and found the 100K resistor was...
Dear Supplier, We are requesting your support to submit IMDS data for the below parts to LACROIX ELECTRONICS IMDS company ID 24959. If you are not the right contact for IMDS, please direct us to the correct person for IMDS in your company. Please re...