Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Filters for HDMI

Hello Everyone,We are interfacing HDMI Connectors with a microprocessor such as AM625 or AM62P or RK3568 for use in Industrial HMI Controller environment.We would be using HDMI 2.0 or 2.1 data transfer rates.We plan to use a HDMI companion chip such ...

STUSB1602 PD 3.0

Dear ST, we are using STUSB1602 and STM32F072 MCU for our application DUAL DRP port functionality requirement in application. Hardware is design based on reference of P-NUCLEO-USB-002 development kit. in application one port where Android mobile is c...

khodidas by Associate
  • 711 Views
  • 1 replies
  • 0 kudos

24 bit ADC

We need 24 bit low speed adc, i have found HX710B is low cost and 24 bit----but one big problem is it is chines manufaturer.can we use it for weighing scale with stm32f103 or stm8 series MCU reliably 

BAS-BLEU by Associate III
  • 1585 Views
  • 3 replies
  • 2 kudos

Resolved! Product P.N. from marking

Hi,I have a component (TVS diode I think) with marking MEPY Z805. Please see the attached image.Anyone can help me to get the P.N.?Thanks in advanceBest RegardsJonata

Jonata by Associate
  • 1356 Views
  • 2 replies
  • 1 kudos

Resolved! Program STM8 flash

Can I use "STM32 ST-Link Utility" or "STM32CubeProgrammer" to program STM8MCU flash?If using "STVP", can it automatically detect the STM8MCU type? or require to configure "STVP" for the MCU type to be programmed.

MC33078DT and input common mode voltage

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2). The original can be found below. Hello! Material Model: MC33078DT, used in in-phase proportional amplification circuit, whe...

WuZunMing by Associate II
  • 1937 Views
  • 5 replies
  • 0 kudos