Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bit set/reset timing

Posted on May 18, 2014 at 09:52I am doing some work which requires precise timing and I think the STM8S can do what I need.  In order to prove this I setup a simple program which toggles PD0 in a while loop.I am using the IAR compiler and it compile...

Nevyn by Associate II
  • 1526 Views
  • 1 replies
  • 0 kudos

Controlling PSD I/O-pins on uPSD3354 uC

Posted on May 15, 2014 at 11:18Hi, We need to modify one of our existing company products to be able to be controller by external I/O. The only externally available I/O-signals are the 6 JTAG pins. These JTAG pins are connected to the PLD I/O-Port C...

henk2 by Associate II
  • 891 Views
  • 0 replies
  • 0 kudos

Trying to find ST9 Visual Programmer for EPB

Posted on May 07, 2014 at 23:04Hello, I have an ST92f150-EPB the software installation CD is long gone, and I need to use my programmer. I have been serching for an STVP that will work with my programmer and my ST92F150JDV1QC chips but I can not fin...

spechin by Associate
  • 1785 Views
  • 2 replies
  • 0 kudos

Activation Level

Posted on May 07, 2014 at 02:56I'm using the STM8L101F3 with IAR. I would like to set and clear the Activation level bit. There is no library function to access this and I'm not sure how to access this register from code. Looking at iostm8l101f3.h, ...

bluscape by Associate III
  • 1195 Views
  • 1 replies
  • 0 kudos

Stm8 touch library

Posted on May 07, 2014 at 09:18I intend to implement a single touch key using stm8 touch library. I am having few issues regarding this.I haven't used the shield concept for noise immunity, so what does a need to define for : SCKEY_P2_DRIVEN_SHIELD_...

STM8s Touch library

Posted on May 07, 2014 at 09:00I intend to use the stm8s touch sensing library, can someone tell me the significance of SCKEY_P1_DRIVEN_SHIELD_MASK , given in the stm8_tsl_conf.h file.Thank you #stm8s-touch-sensing #stm8s-discovery

STM8L151F3 Bootloader

Posted on June 24, 2013 at 13:13Hello! Have anybody any information on bootloader interface configuration for I couldn't find direct instructions on port connections. I assume they should be PC2 and PC3 pins (due to SYSCFG->RMPCR1 default value) but...

beatle7 by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

STVD And Cosmic And assert() Macro

Posted on May 05, 2014 at 08:50If I get...  #error cpstm8 pins_stm8s.c:28(4) missing prototypeon an...  assert( pPin->pPio == GPIOA );even though the file contains...  #include <assert.h>what have I missed/messed?Thank you.

Workalot by Associate III
  • 815 Views
  • 1 replies
  • 0 kudos

AC/DC Transformer help

Posted on April 17, 2014 at 19:55Wurth has ready transformers for AC/DC supplies for 12V, 24V and 48V for 150W, 200W and 250W ratings. The details can be found here: http://katalog.we-online.de/en/pbs/WE-LLCR?sid=f6723a16ca Can these be used readily...

ravindra by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos

STVD - ''Go to Definition Of'' problem

Posted on April 28, 2014 at 17:10Hello, I have installed STVD 4.3.5 with Cosmic STM8 32K Special Edition Free license. I have a problem using feature: Go to Definition Of ''something''. When I try to click this on some function or variable error mes...

bogusz by Associate II
  • 835 Views
  • 0 replies
  • 1 kudos