Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unused pins of STMicro ICs

Hi Masters,I'm not sure if I'm posting on the right section but I can't seem to get a reply from the Legacy MCUs section.I have an STDP6038 but I'm not planning to use the HDMI inputs. What am I supposed to do to the unused HDMI/DP pins? Should I lea...

Resolved! Problem compiling in STVD

Posted on January 19, 2018 at 18:53Hello, I am modifying the code of an STM8S003 that already works.But the code stopped working, even though I have not made any changes yet.The STVD displays the following error message:#error clnk Debug\ajk_strobo_...

I'm using the STM8S003 and I've to change the default value of the option byte AFR0. This operation is easy using a programmer but I'd like to insert this procedure in the source code. Is it possible? Some examples ? Thanks,

Hi everyone,I'm using the STM8S003 and I need to use the alternate function of PC5 so I've to change the default value of the option byte AFR0.This operation is easy using a programmer (ex. STVP) but I'd like to insert this procedure in the source co...

ABarb.17 by Associate
  • 1272 Views
  • 2 replies
  • 0 kudos