Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I need a suitable replacement for the STS25NH3LL

Can anyone suggest a suitable alternative to the STS25NH3LL power MOSFET?  I have been using these for H-bridge control of a brushless DC motor but can get hold of them anymore.  I don't want to re-design the board so it needs to have the same SO-8 p...

CWalk by Associate
  • 575 Views
  • 0 replies
  • 0 kudos

I need help with CAN BUS Driver.

Good day to all,I have STM8Adiscovery and i'm trying to load example from StdPh for the Can Bus but it's not working at all. Development tool IAR for STM8. What I have - as i see from the beggining, program try to send data 2 times - and then Can bus...

ASafo.8 by Associate
  • 870 Views
  • 0 replies
  • 0 kudos

How to choose the right Development Board?

Hello, First of all I would like to apologized for asking this. As i am new to this environment and I know some of you feels annoyed for this.I did aware of programming in Arduino. in my application I used Arduino but suddenly due to some technical l...

DAghe by Associate
  • 935 Views
  • 1 replies
  • 0 kudos

Low-Side Driver L9825

HiI'm using L9825 in one of my applications and have couple of questions just to make sure I get it right:1- I have Vcc=3.3v and Reset line pulled high. Is that ok?2- my understanding is that NON1 and NON2 can be used to directly drive OUT1 and OUT2 ...

HIsma by Associate
  • 863 Views
  • 0 replies
  • 0 kudos

Failed to start GDB in STM8 STVD

Posted on July 25, 2016 at 09:36It is very strange for me that I can't debug today with STM8 STVP v3.9 for the STM8AF Discovery Demoboard. It is always successful before that.The error message shown below:''Failed to launch child process:<gdb.exe>>e...

I'm using a STM8S003F3 and in my project I need to use a secound UART ( using others PINS different that 2(TX) and 3 (RX) ), like a AltSerial Library for Arduino. Somebory knows some similary LIbrary for STM8S003 to perform that function

I'm starting to use STM family, so I haven't much experiency, and I'm Brasilian, so don't borry with my English, Please. Thanks for some help. Best regards

ASant.12 by Associate
  • 1589 Views
  • 2 replies
  • 0 kudos

we are using wifi module SPWF001A, now we wants to implement the HTTPS secured protocol.But in modules AT command literature ,the commands are for HTTP only. Will HTTP command valid for HTTPS also.

we have completed the prototype functional testing and 150 pilot batch is in progress, before going to mass production(2000 Nos ) we need to implement the security protocol.

VKuda by Associate
  • 1131 Views
  • 1 replies
  • 0 kudos